show the entry list
PROFIBUS general -- Configuring and programming communication -- Using communication blocks
Transfer of analog values from and to the PROFIBUS DP slave
Which entries deal with consistent data in conjunction with distributed I/O?
How can you access consistent data without SFC14/15 as part of the process image?
Why does my new CPU 315-2DP (Order No: 6ES7 315-2AG10-0AB0) not process the SFC13 correctly?
How do you receive an alarm with the SFB 54 "RALRM" in compliance with DPV1?
DP slave lifelist using SFC51 "RDSYSST" instead of SFC12 "D_ACT_DP"
Can you use the "Signal System Error" function, the FB126 function block and the SFC13 "DPNRM_DG" system function simultaneously?
Notes for the use of the system function SFC12 "D_ACT_DP"
What is consistent data?
How do you read data consistently from a DP standard slave/PROFINET IO device and write it consistently to a DP standard slave/PROFINET IO device?
Disabling DP slaves after startup of the CPU
Diagnostics information of the FB125 with disabled DP slave
Enabling a disabled DP slave with SFC 12 "D_ACT_DP"
Parameter assignment of SFC 103 / SFC 59 required for identifying and reading out topology data
What are the requirements for using the "Prepare cable diagnostics" function?
Can you use the "Signal System Error" function, the FB126 function block and the SFC13 "DPNRM_DG" system function simultaneously?
Part number:

The "Signal System Error" function and the FB126 "PNIODiag" function block use the SFC13 "DPNRM_DG" system function to determine slave-specific diagnostics data.

The SFC13 system function works asynchronously, which means that the processing of the function can extend over several SFC calls and, thus, it may also span several CPU cycles. The effect of this, in turn, is that there may be several SFC13 jobs active per CPU at the same time. However, the number of SFC13 calls active simultaneously may not exceed a CPU-specific limit. The table below shows the number of jobs that may be active simultaneously.
 
CPU Number of calls
S7-300 4
S7-318 8
S7-400 8
Table 01: Number of SFC13 calls active simultaneously

Consequently, you can use the functions mentioned above simultaneously. However, you must ensure that the maximum number of SFC13 calls active at any one time does not exceed the values specified in Table 1.

The download of FB126 "PNIODiag" is available in Entry ID: 26996747.

Note
More information about system function SFC13 "DPNRM_DG" is available in the manual "System and Standard Functions for S7-300/400 Volume 1 and Volume 2" in Entry ID: 44240604 and in the STEP 7 Online Help.

 Entry ID:17858394   Date:2012-05-14 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour