Special characters in STEP 7:
From STEP 7 V5.2 you can enter special characters for documentation purposes or as a comment without any restrictions.
If you are using a version of STEP 7 < V5.2, then it might not be possible to enter special characters directly in every STEP 7 application. For example, in STEP 7 V5.1 it is possible to enter special characters directly in comment fields in the HW Config, but not in block or network comment fields in the LAD/FBD/STL editor.
In this case you can enter the special characters via the relevant ASCII codes. To enter characters via their ASCII codes you must press and hold the ALT key and enter the relevant code via the numbers keypad.
Please note that you cannot use special characters in every input field. For example, special characters are not usually permitted in tag names.
@ <ALT> + <64>
[ <ALT> + <91>
\ <ALT> + <92>
] <ALT> + <93>
{ <ALT> + <123>
| <ALT> + <124>
} <ALT> + <125>
~ <ALT> + <126>
The download contains the complete ASCII table in PDF format.
ASCII_char_map.pdf ( 20 KB )
|