show the entry list
Which PROFIBUS-PA field devices are supported by AS x88/TM?
Part number:

QUESTION:
Which PROFIBUS-PA field devices are supported by the AS x88/TM and
which drivers do exist for them?

ANSWER:
Any PROFIBUS-PA field device that permit a baud rate of 45.45 kbits/s to be
selected may be used via the DP/PA Siemens bus coupler units. In order to make the
PROFIBUS-PA configurable with COM PROFIBUS, the baud rate of 45.45 kbits/s
must be approved in its GSD file.

If the DP/PA link IM 157 is used, the following PA units with simple configuration
are supported:
• SITRANS P (Siemens)
• SITRANS T3K (Siemens)
• SITRANS F (Siemens)
• SIPART PS2 (Siemens)
• Cerabar S (Endress + Hauser)
• E+H Prosonic T (Endress + Hauser)
• E+H Deltapilot S (Endress + Hauser)
• E+H Deltabar S (Endress + Hauser)
• E+H TMD834 (Endress + Hauser)
• E+H Micropilot II (Endress + Hauser)
• E+H MYCOM CPM (Endress + Hauser)
• E+H MYCOM CLM-ID (Endress + Hauser)
• E+H MYCOM CLM-CD (Endress + Hauser)
• E+H Promag 33 (Endress + Hauser)
• E+H Promass 63 (Endress + Hauser)
• E+H Prowirl 77 (Endress + Hauser)
• Buerkert 6520 (Bürkert)
• Buerkert 8642 (Bürkert)
• IFC090/DPE (KROHNE)

Any other PROFIBUS-PA units must be declared using special entries in the
configuration list. The parameters must be taken from the GSD file of the PA unit.
The following parameter entry in the GSD file is required before a PA unit can be
used via the DP/PA link IM 157:
User_Prm_Data_Len = 3
User_Prm_Data = 0, 0, 0
This PNO recommendation is fulfilled for the majorities of the available PA units.

The PA driver blocks PAAI, PAAO, PADI and PADO of the AS x88/TM-PA
communication software can be used for controlling and monitoring the cyclic data
of all PA units. No additional drivers are required.

 Entry ID:17742909   Date:2003-12-15 
I regard this article....as helpfulas not helpful                                 
related links
SINUMERIK 840D sl Manual
SIPART DR 24 - Serial SIPART 6DR2 ...
SIMATIC S5 CP 544
DCP – Interface for Dynavert L, ...
SIMATIC NET Installation Instruct ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour