show the entry list
ES - SIMATIC Manager -- Product information – System description
What are the options for implementing the security products SCALANCE S, CP443-1 Advanced and CP1628 in the PCS 7 environment?
How do you procure documentation for PCS 7 V8.0 (former Manual Collection DVD)?
How are the licenses for the AS and OS counted as from PCS 7 V7.0?
What actions lead to loss of "AS RT PO" licenses with PCS 7?
What are the requirements for using the CPU_RT block with PCS 7 V7.0?
Important notes on the documentation for PCS 7 V7.0 SP1
Acknowledgement-triggered reporting of SIMATIC PCS 7 V6
Compilation of frequently asked questions about PCS 7 V6.0
How do you install an OPC application for operation in the "SIMATIC HMI" user group?
MS Windows 2000 settings for OS client / supplement to the SIMATIC PCS 7 V6.x Readme file
Correction of the english SIMATIC PCS 7 V6.0 Readme
How do you count the number of process objects (PO) for the PCS 7 licenses?
Which details does Technical Support need regarding inquiries on SIMATIC PCS 7?
Full-text search in the electronic manuals SIMATIC PCS 7 V6.0
What are the options for redundancy and high availability in PCS 7 V6.1 SP1?
Full-text search in the electronic manuals SIMATIC PCS 7 V6.0
Part number:

QUESTION:
Why does the full-text search in the electronic manual SIMATIC PCS 7 V6.0 (MLFB 6ES7650-0XX06-8YX8) possibly not find all the information available?

ANSWER:
If on the index page of the electronic manual CD SIMATIC PCS 7 V6.0 the full-text search is opened to search the CD for a certain term, first of all a dialog window opens. In this dialog window, the search term must be entered and all other settings for the full-text search must be implemented.

Attention:
This setting option is only provided in the English user interface of the Adobe Acrobat Reader. The search e. g. in the German Text of the manuals is not affected by this and works properly. If necessary, change the default user language in Adobe Acrobat Reader.

Please choose the following settings:

  • Turn off the option "Word Stemming".
  • Set the option "Sounds Like".



Fig. 1: Settings of the options for the full-text search on the electronic manual CD

Example:
You are looking for the term "simulation" without the option "sounds like". As a result, 15 manuals/places of use will be found. After activation of the option "Sounds like", the result of the full-text search will improve to 36 manuals. With the option "Word Stemming" activated and "Sounds like" deactivated, you will get 0 results.

Keywords:
Documentation, manual CD


 Entry ID:17738450   Date:2003-11-26 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour