Configuration Notes: The following table gives you an overview of the SIMATIC S7 modules that support the "Direct Data Exchange" function (internode communication) as I slave or DP master in the receive and send area.
| Module |
I slave |
DP master |
| S7-300 CPUs |
x |
x |
| S7-400 CPUs |
x1) |
x1) |
| ET200 CPUs |
|
|
| BM147-1 CPU |
x |
x |
| BM147-2 CPU |
x |
x |
| IM151-7 CPU |
x |
x |
| IM151-7 CPU FO |
x |
x |
| IM151-7 F-CPU |
x |
x |
| IM154-8 CPU |
x |
x |
| PROFIBUS CPs |
|
|
| CP342-5 |
- |
- |
| CP443-5 EXT |
- |
x |
| S7-400 IM modules |
|
|
| IM 467 |
- |
x |
| IM 467 FO |
- |
x |
| WinAC RTX 2005 from SP2 |
- |
x |
x1) The "Direct Data Exchange" function is supported in Send mode from V3.0 and from in Receive mode from V1.1.
Note:
When implementing interface modules, support of the "Direct Data Exchange" (internode communication) function depends on the CPU used and not on the interface module itself.
|