show the entry list
WinCC -- Configuring Tag Logging -- Parameterizing Tag Logging
How can you increase the timeout for starting and terminating Alarm Logging / Tag Logging?
In WinCC, how can you assign the functions of the toolbar buttons of Online Trend Controls to external buttons?
Why, when you select the curve window with the "Read data immediately from archive" option activated, isn't there any data displayed?
What Smart Tools are there for WinCC?
What are the different types of tags available under licensing law?
Why are archive tags not deleted in the Tag Logging editor ?
What does parameter "Supplying tags" mean for a process tag in Tag Logging?
How can you make changes to the project on the configuration computer while the existing process values continue to be acquired and archived on the customer computer?
How can you set the archiving parameters of multiple archive tags at the same time?
Which changes can be made when configuring WinCC Tag Logging?
How can you achieve archiving cycles of less than 500ms in WinCC Tag Logging?
How can you use process-driven archiving in WinCC for a process tag with SFB37 (AR_SEND)?
How do you use SFB37 (AR_SEND) for process-driven archiving of process values in WinCC Tag Logging archives?
What does parameter "Supplying tags" mean for a process tag in Tag Logging?
Part number:

Description
If the option "Supplying tags > System" is enabled, the WinCC tag data is transferred automatically to the archive.
If the option "Supplying tags > Manual input" is enabled, data input in the tag is manual.


Fig. 1: Settings for supplying tags

Note
The internal structure for assigning parameters to archive tags has changed as from WinCC V6.2. The input interface has also been changed accordingly. This does not affect any information contained in the FAQ about supplying tags.


Fig. 2: Settings for supplying tags from WinCC V6.2 onwards.

 Entry ID:17551863   Date:2010-04-19 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour