show the entry list
Industrial Ethernet PC software -- Configuring and programming communication -- Configuring connections
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S5, S7 and PC modules in the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via Industrial Ethernet in the SIMATIC NET Quick Start Collection?
Which hardware and software is required in the WinCC system to communicate with an S7 via a CP343-1?
How do you use the variable symbols defined in STEP 7 with the OPC server of SIMATIC NET?
How do you configure S5-compatible communication to the SIMATIC S5 for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure S5-compatible communication to the SIMATIC S7 for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure a PC station as PROFINET IO controller for connecting to a S7 station (as PROFINET IO device) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
Establishing a connection from a PC to the S7-400 
How do you configure an S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software?
What should I watch out for when using an "S/R OPC Server" in the Fetch/Write service mode?
How do you configure S5-compatible communication to the SIMATIC S7 via Industrial Ethernet for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you set up a Fetch/Write connection (S5-compatible communication) to the SIMATIC S5 via Ethernet for the SIMATIC NET OPC server with the SIMATIC NET CD 07/2001 or higher?
How do you configure S5-compatible communication to the SIMATIC S5 via Industrial Ethernet for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure a fault-tolerant S7 connection for the SIMATIC NET OPC server via Industrial Ethernet with the SIMATIC NET PC software?
How do I create a Fetch/Write-connection (S5-compatible communication) to SIMATIC S7 for the SIMATIC NET-OPC Server via Ethernet with the SIMATIC NET CD 07/2001 or higher?
How do you configure an S7 connection via Industrial Ethernet with the SIMATIC NET OPC server and the SIMATIC NET PC software?
How do you configure a fault-tolerant S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software?
Industrial Ethernet PC CPs -- Configuring and programming communication -- Configuring connections
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC PC modules by way of the Industrial Ethernet using the TCP protocol?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC PC modules by way of the Industrial Ethernet using the ISO transport protocol?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via Industrial Ethernet in the SIMATIC NET Quick Start Collection?
What differences are there when configuring S7 connections?
How do you use the variable symbols defined in STEP 7 with the OPC server of SIMATIC NET?
How do you configure S5-compatible communication to the SIMATIC S5 for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure S5-compatible communication to the SIMATIC S7 for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure a PC station as PROFINET IO controller for connecting to a S7 station (as PROFINET IO device) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
Establishing a connection from a PC to the S7-400 
How do you configure S5-compatible communication to the SIMATIC S7 via Industrial Ethernet for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you set up a Fetch/Write connection (S5-compatible communication) to the SIMATIC S5 via Ethernet for the SIMATIC NET OPC server with the SIMATIC NET CD 07/2001 or higher?
How do you configure an S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure S5-compatible communication to the SIMATIC S5 via Industrial Ethernet for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure a fault-tolerant S7 connection for the SIMATIC NET OPC server via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure a fault-tolerant S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure an S7 connection via Industrial Ethernet with the SIMATIC NET OPC server and the SIMATIC NET PC software?
Information about "Configuring connections"
PROFIBUS PC Software -- Configuring and programming communication -- Configuring connections
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S5, S7 and PC modules in the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via PROFIBUS in the SIMATIC NET Quick Start Collection?
How do you use the variable symbols defined in STEP 7 with the OPC server of SIMATIC NET?
How do you configure a PC station as DP master for connecting to a DP slave for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an S7 connection for a user application via PROFIBUS with the SIMATIC NET PC software?
How do you configure an S7 connection for the SIMATIC NET OPC server via PROFIBUS with the SIMATIC NET PC software?
How do you configure an S7 connection for a user application via MPI with the SIMATIC NET PC software?
How do you configure an FDL connection to the SIMATIC S5 95-U via PROFIBUS for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an FDL connection to the SIMATIC S7 via PROFIBUS for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an FDL connection to the SIMATIC S5 via PROFIBUS for the SIMATIC NET OPC server with the SIMATIC NET PC software?
Establishing a connection from a PC to the S7-400 
How do you configure a PC station as DP slave for connecting an S7 station (as DP master) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an S7 connection via MPI with the SIMATIC NET OPC server and the SIMATIC NET PC software?
PROFIBUS PC CPs -- Configuring and programming communication -- Configuring connections
Where can you find sample S7 programs and documentation for communication via PROFIBUS in the SIMATIC NET Quick Start Collection?
What differences are there when configuring S7 connections?
How do you use the variable symbols defined in STEP 7 with the OPC server of SIMATIC NET?
How do you configure a PC station as DP master for connecting to a DP slave for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an S7 connection for a user application via PROFIBUS with the SIMATIC NET PC software?
How do you configure an S7 connection for the SIMATIC NET OPC server via PROFIBUS with the SIMATIC NET PC software?
How do you configure an S7 connection for a user application via MPI with the SIMATIC NET PC software?
How do you configure an FDL connection to the SIMATIC S5 95-U via PROFIBUS for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an FDL connection to the SIMATIC S7 via PROFIBUS for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an FDL connection to the SIMATIC S5 via PROFIBUS for the SIMATIC NET OPC server with the SIMATIC NET PC software?
Establishing a connection from a PC to the S7-400 
How do you configure a PC station as DP slave for connecting an S7 station (as DP master) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an S7 connection via MPI with the SIMATIC NET OPC server and the SIMATIC NET PC software?
Information about "Configuring connections"
How do you use the variable symbols defined in STEP 7 with the OPC server of SIMATIC NET?
Part number:

Configuration notes:
In version V6.1 of SIMATIC NET (CD 11/2002) and higher you can use the symbol table and the data block symbols of your STEP 7 project as a basis for generating the symbols of the SIMATIC NET OPC server.

This entry describes how to generate symbols for the SIMATIC NET OPC server from the STEP 7 symbol table.

A PC station with a standard Ethernet network card is used. Data exchange between PC station and S7 station is implemented via Industrial Ethernet using S7 Communication.

Requirements:
Both PC station and S7 station must be configured in the same STEP 7 project.

Configuration of the S7 station:
Use the SIMATIC Manager to open your STEP 7 project that contains the SIMATIC S7 station.


Fig. 01: STEP 7 project

Switch to the S7 program folder and double-click on "Symbols". The symbol table opens.

In the symbol table you define the symbol names you want.


Fig. 02: Symbols in the symbol table

Other variables with symbol names of the STEP 7 project are in the existing data blocks - DB1 in this example.


Fig. 03: Variables in DB1

Download the hardware configuration and the user program to the CPU of your S7 station.

Configuring the PC station:
You insert a new PC station via the menu Insert -> Station -> SIMATIC PC Station.


Fig. 04: Inserting a PC Station

Please follow the instructions given in Entry ID 15355168 for configuring the PC station.

Incorporating STEP 7 symbols in the OPC server:
Then right-click the OPC server and open the Object Properties of the OPC server.


Fig. 05: Opening the Object Properties of the OPC server

In the Properties dialog of the OPC server you switch to the "S7" tab. In this dialog you define which STEP 7 symbols are used in the OPC server. Enable either the "All" or the "Configured" option.


Fig. 06: Properties dialog of the OPC server - "S7" tab

If you enable the "Configured" option, then you right-click the "Configure..." button. The following dialog opens.


Fig. 07: Configure Symbols dialog - variable symbols in the symbol table


Fig. 08: Configure Symbols dialog - variable symbols in the data block

In the "Configure Symbol" dialog you can make the variable symbols defined in the symbol table and data block visible for the OPC server and define their authorization (Read/Write, Read, Write or none).

Click the "OK" button to close the "Configure Symbols" dialog.

Then, in NetPro, you mark the PC station and save and compile the complete configuration.


Fig. 09: Saving and compiling the configuration

Mark your PC station.


Fig. 10: Save and Compile

If warnings are displayed when saving and compiling the configuration, then they should be treated as purely information. It is possible to download the configuration into the PC station. If errors occur when saving and compiling, it is not possible to download the configuration into the PC station.

In NetPro, you mark the PC station and click on the "Download" button to download the configuration into the PC station.

The following message reminds you that the downloading procedure will delete the data already on the components concerned and the new data will be downloaded to them.


Fig. 11: PLC download

Acknowledge the message with "OK". Now the download starts.
First the target modules are stopped. Acknowledge the subsequent message with "OK" to continue the download procedure.


Fig. 12: Stopping the target modules

Note:
The following entry provides information on possible causes of error messages during the downloading procedure 12033912.

Successful downloading completes configuration of the PC station.

Use the OPC Scout to check whether the STEP 7 symbols are available in the OPC server. This OPC client is included in the SIMATIC NET PC software.

Start the OPC Scout in the Windows START menu via SIMATIC -> SIMATIC NET -> OPC Scout.

Double-click on "OPC.SimaticNET" to connect to the SIMATIC NET OPC server.


Fig. 13: Connecting to the SIMATIC NET OPC server

In the dialog box that opens you enter a group name of your choice.


Fig. 14: Entering a group name

Double-click on the group name created, "S7" in this example, to open the OPC Navigator. In the OPC Navigator you can define the OPC items.


Fig. 15: Opening the OPC Navigator

The incorporated STEP 7 symbols are to be found in the OPC Navigator in the "...\SYM" folder.
Double-click on "\SYM". The S7 station from the STEP 7 project is displayed. This contains more subfolders (CPU and data blocks).
The variable symbols that you defined in the STEP 7 symbol table are contained in the CPU folder. Mark the CPU folder. The defined variable symbols are displayed in the middle window pane. Mark the variable names and click on the "->" button to add them to the OPC item list. Click "OK" to close the dialog. 

The variable symbols defined in the data block are in the data block folder.


Fig. 16: OPC Navigator

The OPC Scout has added the selected variables with symbolic names to the list of OPC items.
If the quality of the OPC items is good, then the communication connection can be set up and you can read/write the values of the OPC items.


Fig. 17: List of OPC items

 Entry ID:17413251   Date:2008-11-10 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour