show the entry list
PROFIBUS general -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
What should you watch out for when adding components or changing their parameters using CiR (Configuration in Run)?
What should you pay attention to when operating a DP slave temporarily on a PROFIBUS DP network?
How do you connect the SIMATIC Field PG to the bus system to parameterize and diagnose the distributed I/O devices?
Which options are available for configuring the ET 200 stations?
Configuration of the alarm mode in STEP 7 for the diagnostics repeater (6ES7 972-0AB01-0XA0)
Correction to bus time calculations
Basic knowledge for configuring PROFIBUS-DP networks
What are the conditions for assigning the addresses of I/O modules (central or distributed) to an S7 CPU?
Cyclic program processing only once all the DP stations have signaled that they are finished
Which parameters must be taken into account when planning an electrical network?
How can you calculate the bus cycle time on the PROFIBUS DP with STEP 7?
Configuration of the alarm mode in STEP 7 for the diagnostics repeater (6ES7 972-0AB01-0XA0)
Part number:

QUESTION:
Which mode do I have to adjust at the diagnostics repeater, in order to call the organization block OB82?

ANSWER:
If the diagnostics Repeater is run with DPV1 mode at a S7 CPU, the DP alarm mode of the repeater has nevertheless to be set to DPVO in STEP 7. The diagnostics alarm OB (OB82) will then be called continously in the S7-CPU.

In the register "Parameter assignment" in the object properties of the diagnostics repeater, the "DP-alarm mode" can be set.

Choosing the DPV1 mode, the diagnostics alarm OB (OB82) will not be called in case of diagnostics occurences in the S7 controller. Therefore it is recommended to keep the pre-adjustment DPV0.

Note:
Further notes about the configuration can be found in chapter 6 "Commissioning" of the manual "SIMATIC diagnostics repeater for PROFIBUS-DP" under entry-ID: 7915183.

Keywords:
Watchdog interrupt, Hardware configuration


 Entry ID:17119245   Date:2003-09-29 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour