show the entry list
SIMATIC BATCH option -- Setting up development environments -- Parameterizing systems
Why can you not import materials in SIMATIC BATCH?
How can you avoid DCOM errors in the Windows event viewer when using power users?
Empty BOM after starting the BOM via the desktop icon
Which interface to MES/ERP offers SIMATIC Batch?
Modification of the IP-Adress in CCAgent in SIMATIC PCS 7 V6.0
Which releases and access rights are necessary for all BATCH users?
Which interface to MES/ERP offers SIMATIC Batch?
Part number:

Description
The option package API interface to SIMATIC BATCH, offers the possibility to connect online and offline functions of SIMATIC BATCH directly to an OEM system or to a MES/ERP application of your choice. 

The API interface offers both: a C interface (data format CSV) and a COM connection (data format XML). 

Further information about the use and configuration possibilities can be found at the Readme and the on-line help for the option software "API interface".

Note
At the use of Simatic IT framework the option "API interface" is also necessary.

 Entry ID:16842807   Date:2010-11-02 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour