show the entry list
ES - SIMATIC Manager -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How do the PCS 7 channel blocks behave in the case of a short-circuit to ground of an encoder supply on the digital input module SM321 (6ES7 321-7TH00-0AB0)?
How can you change the size of the available free main memory of a SIMATIC S7-400 CPU?
Why is the active bus module IM153 (6ES7195-7HB00-0XA0) not listed in the English PCS 7 V6.1 documentation?
How do you use a watchdog module of an ET200iSP in PCS 7?
How can I read out the current module status of a SIMATIC Station?
Moving DP slaves to a different master system
How do you start up a SIMOVERT Master Drive SC in PCS 7 V4.0x?
How can you save the configuration of a CP 341 with retroloadable drivers without an online connection to the CPU?
Channel drivers and module drivers in PCS 7 V5.2 for ET 200iS
Why is the system data inconsistent after the CPU has been configured as time slave in HW Config?
Operating master systems (DPV1- and S7-compatible) in one rack
Module driver PA_AI (in PCS 7 V5.2) can only be used to connect IM 157 with MLFB 157-0AA81.. and 157-0AA80..
Selection tool for I/O modules in SIMATIC PCS 7
What should you watch out for with the hardware configuration of the AS CPU?
Configuration of DP slaves
Note on configuring the ET200X (6ES7 141-1BF30-0XB0)
Non-volatile effect with an ET 200M in PCS 7 V5.x
What statuses can the ET 200M outputs have in CPU STOP?
Configuration of Diagnostics Repeater in PCS 7 V6
Diagnostic Alarms of Digital Input Blocks SM 321-7BH00 and SM 321-7BH01
How do you connect a DPV1-compatible PA field device after a DP/PA link DPV1 in PCS 7?
How can you avoid messages with "old" time stamps when commissioning a PLC?
Operating master systems (DPV1- and S7-compatible) in one rack
Part number:

QUESTION:
What are the requirements for operating multiple DP master systems in one S7-400 rack with different profiles (DPV1- and S7-compatible)?

ANSWER:
The hardware and software requirements for mixed operation of PROFIBUS profiles DPV1- and S7-compatible in the same rack are as follows:

  • S7-400 CPU with firmware version V3.1.0 or higher
  • When using a CP 443-5 Extended, MLFB 6GK7 443-5DX03-0XE0 as of firmware version V5.0
  • STEP 7 V5.2 or PCS 7 V6 and higher


 Entry ID:16820988   Date:2003-09-05 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour