Instructions:
In this example, a CP1613 is used for the S5-compatible communication via the OPC server with an S5 controller on the Industrial Ethernet network.
Note:
The same procedure also applies for communication processors CP1613 A2, CP1612, CP1512 and other standard network cards.
General Information: You can choose between two different configuration tools:
- NCM PC: NCM PC is supplied with the SIMATIC NET CD and permits you to create PC projects and open STEP 7 projects. However, it is not possible to use this software to edit the S7 blocks in the STEP 7 project.
- STEP 7: STEP 7 is a separate software package and permits you to create S7-400, S7-300 and PC projects. It is possible to use this software to edit the S7 blocks.
Only one of these tools can be installed.
Please follow the instructions below for configuring the PC station.
Guide_SRS5_OPC_e.pdf ( 2130 KB )
Keywords: Send/Receive connection, SIMATIC Net PC software, Configuration, Guideline, OPC server, S7-1613, SOFTNET S7, ISO transport connections
|