show the entry list
Industrial Ethernet PC software -- Configuring and programming communication -- Configuring connections
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S5, S7 and PC modules in the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via Industrial Ethernet in the SIMATIC NET Quick Start Collection?
Which hardware and software is required in the WinCC system to communicate with an S7 via a CP343-1?
How do you use the variable symbols defined in STEP 7 with the OPC server of SIMATIC NET?
How do you configure S5-compatible communication to the SIMATIC S5 for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure S5-compatible communication to the SIMATIC S7 for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure a PC station as PROFINET IO controller for connecting to a S7 station (as PROFINET IO device) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
Establishing a connection from a PC to the S7-400 
How do you configure an S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software?
What should I watch out for when using an "S/R OPC Server" in the Fetch/Write service mode?
How do you configure S5-compatible communication to the SIMATIC S7 via Industrial Ethernet for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you set up a Fetch/Write connection (S5-compatible communication) to the SIMATIC S5 via Ethernet for the SIMATIC NET OPC server with the SIMATIC NET CD 07/2001 or higher?
How do you configure S5-compatible communication to the SIMATIC S5 via Industrial Ethernet for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure a fault-tolerant S7 connection for the SIMATIC NET OPC server via Industrial Ethernet with the SIMATIC NET PC software?
How do I create a Fetch/Write-connection (S5-compatible communication) to SIMATIC S7 for the SIMATIC NET-OPC Server via Ethernet with the SIMATIC NET CD 07/2001 or higher?
How do you configure an S7 connection via Industrial Ethernet with the SIMATIC NET OPC server and the SIMATIC NET PC software?
How do you configure a fault-tolerant S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software?
Industrial Ethernet PC CPs -- Configuring and programming communication -- Configuring connections
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC PC modules by way of the Industrial Ethernet using the TCP protocol?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC PC modules by way of the Industrial Ethernet using the ISO transport protocol?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via Industrial Ethernet in the SIMATIC NET Quick Start Collection?
What differences are there when configuring S7 connections?
How do you use the variable symbols defined in STEP 7 with the OPC server of SIMATIC NET?
How do you configure S5-compatible communication to the SIMATIC S5 for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure S5-compatible communication to the SIMATIC S7 for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure a PC station as PROFINET IO controller for connecting to a S7 station (as PROFINET IO device) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
Establishing a connection from a PC to the S7-400 
How do you configure S5-compatible communication to the SIMATIC S7 via Industrial Ethernet for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you set up a Fetch/Write connection (S5-compatible communication) to the SIMATIC S5 via Ethernet for the SIMATIC NET OPC server with the SIMATIC NET CD 07/2001 or higher?
How do you configure an S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure S5-compatible communication to the SIMATIC S5 via Industrial Ethernet for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure a fault-tolerant S7 connection for the SIMATIC NET OPC server via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure a fault-tolerant S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure an S7 connection via Industrial Ethernet with the SIMATIC NET OPC server and the SIMATIC NET PC software?
Information about "Configuring connections"
How do you configure a fault-tolerant S7 connection for the SIMATIC NET OPC server via Industrial Ethernet with the SIMATIC NET PC software?
Part number:

Instructions:
In this example, a CP1613 is used for the S7 communication via the SIMATIC NET OPC server to an S7-400H system on the Ethernet.
The requirement for the procedure described is an existing configuration of the S7400-H system with network connection.

Warning:
Fault-tolerant S7 connections are available exclusively in CP1613 (6GK1161-3AA00), CP1613 A2 (6GK1161-3AA01) and CP1623 (6GK1162-3AA00). If you use a CP1613 A2 or CP1623 then these modules must be configured as CP1613 in the STEP 7 hardware configuration.
It is not possible to use standard network cards in this case.

General information:
The requirement is that one of the two following configuration tools is installed on the Engineering Station.

  • NCM PC: 
    NCM PC is supplied with the SIMATIC NET CD and permits you to create PC projects and open STEP 7 projects. It is not possible to use this software to edit the S7 blocks in the STEP 7 project. 
  • STEP 7:
    STEP 7 is a separate software package and permits you to create S7-400, S7-300- and PC projects. It is possible to use this software to edit the S7 blocks.

Note:
You need an Engineering Station with STEP 7 for commissioning the PC station. STEP 7 is mandatory for configuring a fault-tolerant S7 connection between PC station and S7400-H system.
You need the license for the SIMATIC NET PC software S7-REDCONNECT on the PC station that communicates with the S7400-H system via fault-tolerant S7 connections.

Please follow the instructions below for configuring the PC station.

Guide_S7_H_OPC_e.pdf ( 1626 KB )

More information on communication with S7-400H systems is available in the manual "S7-400H" in Entry ID 1186523. Refer in particular to the information on communication with the OPC server in section 11.8 "General Information on Communication".

Keywords:
OPC server, CP1613, CP1623, Fault-tolerant S7 connection, Guidelines, REDCONNECT

 

 Entry ID:16651010   Date:2008-06-18 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour