Instructions:
In this example, a CP5611 is used for the communication via the OPC server as DP slave with an S7 station as DP master on the PROFIBUS.
Note: The procedure described here also applies for communication processors CP5511, CP5512 and CP5621.
General information: You can choose between two different configuration tools:
- NCM PC:
NCM PC is supplied with the SIMATIC NET CD and permits you to create PC projects and open STEP 7 projects. However, it is not possible to use this software to edit the S7 blocks in the STEP 7 project.
- STEP 7:
STEP 7 is a separate software package and permits you to create S7-400, S7-300 and PC projects. It is possible to use this software to edit the S7 blocks.
The requirement is that STEP 7 is installed and that the DP master is already configured (for example, STEP 7 project with the configuration of an S7 station). If the DP master is also a PC station, then the configuration of the PC station as DP slave can also be made with NCM PC.
Please follow the instructions below for configuring the PC station.
Guide_DPSlave_e.pdf ( 1366 KB )
More information on using and configuring a PC station as DP slave or DP master is available in the applications listed below:
| Title of application |
Entry ID |
| Distributed Automation with the PC - The SIMATIC NET OPC Server as PROFIBUS DP Slave |
21040390 |
| Controlling with the PC - The SIMATIC NET OPC Inproc Server as DP Master |
21045282 |
Keywords:
DP-Slave, CP5611, CP5511, CP5512, CP5621, Hardware Configuration, SIMATIC NET PC software, Configuration, Guidelines, SOFTNET DP slave, Link DP slave, PC station.
|