|
Instructions This value is dependent on the conversion time, the type of measurement (current, voltage and resistance measurement) and the number of active channels.
The total conversion time determined (basic conversion time + additional conversion times) for a channel has to be multiplied by the number of active channels. This gives you the cycle time for a module. A signal must be present for at least this time to ensure that it is recognized as a process alarm.
The following manuals give information on the length of the basic conversion times of the various modules and on any additional conversion times that might have to be taken into account
| Modules |
Manual |
Entry ID |
| ET200M |
SIMATIC S7-300 programmable logic
controller, module data |
8859629 |
| ET200S |
SIMATIC ET 200S distributed I/O system
|
1144348 |
| ET 200iSP |
SIMATIC ET 200iSP distributed I/O device |
28930789 |
| ET 200pro |
SIMATIC ET 200pro distributed IO system |
21210852 |
| ET 200eco PN |
SIMATIC ET 200eco PN distributed I/O device |
29999018 |
If smoothing of the input signals has also been configured, the smoothing level which has been parameterized has to be taken into account. The smoothing levels (weak, medium and strong) are multiples of the cycle time and vary depending on the module used.
The smoothing level attenuates the rise of an input signal. The specification in cycles indicates in how many cycles an input signal with 63% of its maximum value is recognized
Note
Refer to the manuals listed above to find out the number of cycles per smoothing level for your module.
|