show the entry list
ET 200pro -- Product information -- Technical data
How long does the input signal have to be present before an analog input module identifies this signal as a process alarm?
Which CPU can you operate as a PROFINET I device?
What are the requirements for using the S7 routing function and which modules can you implement?
What is the significance of the IP protection classes IP65, IP66, IP67?
ET 200iSP -- Product information -- Technical data
Which PROFIBUS connectors can you use in Zone 1 or 2?
Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gas
How do you assign and identify thermocouples?
How long does the input signal have to be present before an analog input module identifies this signal as a process alarm?
ET 200M (standard modules) -- Product information -- Technical data
Which modules can you use when implementing software redundancy?
Which SIMATIC S7 components and which drives support clock-synchronicity functionality?
Multiline set-up of ET200M
How many modules can you operate with one interface module of the ET 200M?
Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gas
How do you assign and identify thermocouples?
How long does the input signal have to be present before an analog input module identifies this signal as a process alarm?
ET 200S (standard modules) -- Product information -- Technical data
What are the requirements for using the S7 routing function and which modules can you implement?
Which communication services supported by the CPUs with integrated PROFINET interface and by the WinAC RTX via Industrial Ethernet?
Which PROFIBUS connectors can you use in Zone 1 or 2?
What are the system limits in an F CPU for safe bidirectional data communication via S7 Communication?
Which SIMATIC S7 components and which drives support clock-synchronicity functionality?
ET 200S: Are there special requirements for ET200S when mounted on sheet metal plates?
ET200S: How many motor starters can be allocated to a power module?
ET 200S: How many motor starters can be allocated to a power module?
ET 200S: How many load feeders may be connected?
Calculating the maximum absolute error of the counter module 1Count24V/100kHz (6ES7 138-4DA02-0AB0) when measuring rotational speed
Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gas
Baud rates for ET200S FO modules
Maximum power load for digital output modules
Minimum distance to the ET 200S front
How do you assign and identify thermocouples?
How long does the input signal have to be present before an analog input module identifies this signal as a process alarm?
ET 200eco -- Product information -- Technical data
Which temperature ranges and environmental conditions apply for the outdoor use of ET 200eco PN?
How long does the input signal have to be present before an analog input module identifies this signal as a process alarm?
What is the significance of the IP protection classes IP65, IP66, IP67?
In what way are ET 200eco and ET 200pro resistant to chemicals?
How long does the input signal have to be present before an analog input module identifies this signal as a process alarm?
Part number:

Instructions
This value is dependent on the conversion time, the type of measurement (current, voltage and resistance measurement) and the number of active channels.

The total conversion time determined (basic conversion time + additional conversion times) for a channel has to be multiplied by the number of active channels. This gives you the cycle time for a module. A signal must be present for at least this time to ensure that it is recognized as a process alarm.

The following manuals give information on the length of the basic conversion times of the various modules and on any additional conversion times that might have to be taken into account 
 
Modules Manual

Entry ID

ET200M  SIMATIC S7-300 programmable logic
controller, module data
8859629
ET200S  SIMATIC ET 200S distributed I/O system 
1144348
ET 200iSP SIMATIC ET 200iSP distributed I/O device 28930789
ET 200pro SIMATIC ET 200pro distributed IO system 21210852
ET 200eco PN SIMATIC ET 200eco PN distributed I/O device 29999018

If smoothing of the input signals has also been configured, the smoothing level which has been parameterized has to be taken into account. The smoothing levels (weak, medium and strong) are multiples of the cycle time and vary depending on the module used. 
The smoothing level attenuates the rise of an input signal. The specification in cycles indicates in how many cycles an input signal with 63% of its maximum value is recognized

Note
Refer to the manuals listed above to find out the number of cycles per smoothing level for your module.

 Entry ID:16644634   Date:2011-07-20 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour