show the entry list
WinCC -- Product information -- Information on WinCC Smart Tools
Compatibility Tool for Automation and Drive Technology
With what are SIMATIC WinCC V7.x, V 6.x and V5.x compatible?
EasyLanguage adds a 'T' to empty ToolTips upon export
Display/mask out first page/final page of the Dynamic wizard
Warning "Object has no or empty type property" when using the Export Wizard
Changing communication between WinCC server and client in WinCC V5 SP2
WinCC Configuration Tool: Error message while reading large WinCC-Projects
How can you make the menu item "WinCC" visible again in MS Excel when using the "WinCC Configuration Tool"?
Presetting the maximum number of lines in the WinCC Configuration Tool
How do you install the WinCC Smart Tools?
What Smart Tools are there for WinCC?
WinCC Configuration Tool: Error message while reading large WinCC-Projects
Part number:

QUESTION:
What is the reason for an error message like: "Out of memory" while reading large WinCC-Projects (> 60MB) using the WinCC Configuration Tool?

ANSWER:  
This message is based on a system characteristic of Microsoft Excel.

Microsoft Excel does limit the RAM capacity provided for the work folders. This limitation is about 60MB for Microsoft Excel 2000.  For Microsoft Excel XP, the limitation was raised to ca. 160MB. 

While reading in large WinCC projects with theWinCC Configuration Tool, this limitation might be reached. In this case, Excel triggers out a simple Messagebox "Out of memory". 

Raising the RAM provided by the PC for the work storage does not solve the problem.    

Note:
Please note, that large WinCC Projects under Microsoft Excel XP can only be successfully read  with the WinCC Configuration Tool, once WinCC V5.1 Hotfix 3 had been installed.

 Entry ID:16511562   Date:2003-07-30