show the entry list
WinCC -- Product information -- Information on WinCC Smart Tools
Compatibility Tool for Automation and Drive Technology
With what are SIMATIC WinCC V7.x, V 6.x and V5.x compatible?
EasyLanguage adds a 'T' to empty ToolTips upon export
Display/mask out first page/final page of the Dynamic wizard
Warning "Object has no or empty type property" when using the Export Wizard
Changing communication between WinCC server and client in WinCC V5 SP2
WinCC Configuration Tool: Error message while reading large WinCC-Projects
How can you make the menu item "WinCC" visible again in MS Excel when using the "WinCC Configuration Tool"?
Presetting the maximum number of lines in the WinCC Configuration Tool
How do you install the WinCC Smart Tools?
What Smart Tools are there for WinCC?
EasyLanguage adds a 'T' to empty ToolTips upon export
Part number:

QUESTION:
Why, after importing the updated csv file with EasyLanguage, do all the previously empty ToolTips have a 'T'?

ANSWER:
This behavior occurs in versions of EasyLanguage < V5.0. When the image texts are exported into a csv-file with the EasyLanguage versions concerned, then a 'T' is added to all empty ToolTip fields. The current version V5.0 of EasyLanguage is on the WinCC V5 CD in the SmartTools -> CC_GraphicsTextImportExport path.

If you are using an older version of EasyLanguage and this case occurs, then there is a quick way of getting rid of the "T":

  1. After import, select all the operable objects.
  2. Then remove the ToolTip for all of them together.
 Entry ID:1548652   Date:1999-11-26