show the entry list
FM 353, 354, 453 -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
What must be considered when using the SIMATIC S7 FM354 module with incremental encoder?
What should you watch out for when calling FB POS_CTRL and FB POS_MSRM?
Which function modules (FM) can be used remotely in an ET 200M?
What should you watch out for when parameterizing a digital input for the "Set flying actual value" function in Automatic mode?
How do you assign parameters to an FM354 when using an absolute linear rule?
What does MD38 signify with FM 353?
How can you reduce the positioning times for short distances?
What invokes the procedure program error 0x0801 "Program selection subprogram error"?
How many FM 353s or FM 354s can the communicate with an OP that is connected to the CPU via MPI?
Transferring an NC block (traversing program) by user program to an FM353 / FM354
Aborting an active MDI record of an FM353 or FM354
Behavior of the FM 354 upon signal change at the release input
Behavior of the FM 354 upon signal change at the release input
Part number:

QUESTION:
How does the FM 354 react to a signal change at the release input during travel?

ANSWER:
A digital input is used on an FM 354 as release input (parameters of MD 34 as in Table 9-13 in the manual).
If there is a change of signal at the release input during travel, then you have the following reactions:

  1. Upon signal change from 1 to 0 at the release input the travel is braked.
  • Braking of travel:
    In the modes Tip, Reference point travel, Incremental, MDI and Automatic, the FM 354 brakes with the specified delay (MD 41).
    In the Control mode, the FM 354 reduces the output voltage according to the voltage ramp set (MD 45).
  • Updating the status signals:
    In the modes Tip, Incremental, MDI, Automatic and Control, "Wait for external release" (WFG) is set, all the other status signal remain unchanged. The travel is interrupted and can be continued.
    In the Reference point travel mode, upon axis standstill "Processing in operation" (BL) and the direction signal (FR+ or FR-) are reset and the start release (SFG) is set. The reference point travel is terminated and has to be started again.
  1. Upon subsequent signal change from 0 to 1 at the release input the interrupted travel is continued:
  • In the modes Tip, Incremental, MDI, Automatic and Control, the travel is restarted immediately. For Control and Tip the control signal "Direction" (R+ or R-) must still be present.
  • In the Reference point travel mode, travel is restarted when the start signal is set.

More information on the release input is available in the manual for the FM 354 " FM 354 Servo Drive Positioning Module V4.x" - Entry ID 2110628, sections 9.8 and 9.8.1.


 Entry ID:15309616   Date:2003-09-29 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour