show the entry list
Multi Panel -- Setting up and parameterizing hardware -- Setting up connections
Which ports are used by WinCC Advanced, WinCC Runtime Advanced, WinCC Runtime Professional, Basic Panels, Comfort Panels, Panels and IPC?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Microsoft ActiveSync connection for MP270, MP370
Which hardware can be connected to the USB port of HMI operating devices?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
What connecting cables are there for connections between the operator panels and the different controllers?
How do you connect a panel to a SIMATIC H station?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
How you change / save the size and position of the keyboard on Windows-based operator panels?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
ProTool -- Configuring and programming communication -- Configuring communication to PCs
Connecting the SIMATIC NET OPC server CD11/2002+SP1 to WinAC MP with PROFIBUS
OPC connection to a panel not possible with ProTool V6.0 SP1A
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Construction of an OPC.SimaticHMI.PTPro OPC-Server and a ProTool/Pro Runtime as OPC-Client
WinCC flexible ES -- Configuring and programming communication -- Configuring communication to PCs
Which settings are required in Windows XP SP2 and WinCC flexible for server-client communication via OPC-DCOM?
How can you use a PC to simulate or realize sending e-mails in the case of an HMI station message?
How do you configure the OPC server PC Access in order to operate WinCC flexible Runtime as OPC client?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Which settings are required in Windows 2000, Windows XP, Windows Vista and WinCC flexible for server-client communication via OPC XML?
Which ports are used by WinCC flexible?
How can you access a Microsoft Windows 2003 server with a panel / PC?
How do you integrate an HMI operator panel into a local network?
What options are there in WinCC flexible for using a Multi Panel or Mobile Panel as an OPC server?
What options are there in WinCC flexible 2004 for using a multipanel as an OPC server?
WinAC MP -- Setting up and parameterizing hardware -- Setting up connections
How in WinAC MP 2008 do you program data transfer with the ET200S 1SI module for the 4-byte or 8-byte communication type?
How can WinAC MP exchange data with a PC or PLC?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Connessione di comunicazione fra ProTool Pro e WinAC Pro tramite Computing (WinAC < V3.0)
Connecting the SIMATIC NET OPC server CD11/2002+SP1 to WinAC MP with PROFIBUS
Connection settings for a communication between ProTool/Pro and WinAC
Connecting ProTool/Pro PC-Runtime with Ethernet to a WinAC MP
Mobile Panels -- Setting up and parameterizing hardware -- Setting up connections
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How do you connect a panel to a SIMATIC H station?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Operator controls as DP direct keys on a Mobile Panel 170
Deactivating and Activating of DP Slave Functions on MOBILE Panel 170
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
What connecting cables are there for connections between the operator panels and the different controllers?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
Touch Panel / Operator Panel -- Setting up and parameterizing hardware -- Setting up connections
Which ports are used by WinCC Advanced, WinCC Runtime Advanced, WinCC Runtime Professional, Basic Panels, Comfort Panels, Panels and IPC?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Which hardware can be connected to the USB port of HMI operating devices?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
How do you connect a panel to a SIMATIC H station?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
What connecting cables are there for connections between the operator panels and the different controllers?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Connection of an OP3 on the MPI interface
OP3 - Transfer mode
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Part number:

Instructions:
Using the "File Transfer Protocol" you can move files between a WinCE panel (e.g. MP370) used as an FTP client and a PC used as an FTP server. This entry explains how to configure the FTP server on the PC and how to connect the WinCE panel to this server using the Pocket Internet Explorer. A requirement for this is that you have a correctly functioning Ethernet connection between the two devices created using a cross-over cable or a hub.
The Microsoft Pocket Internet Explorer, which can be optionally transferred to a Windows CE panel using ProSave, only supports downloads from the server. Uploads are not supported.

Contents:

Installation and configuration of the FTP server in Win2000 Server
The table below describes all the steps that are required in order to set up an FTP server in "Microsoft Windows 2000 Server".
 
No. Procedure
1 Adding Windows components
  • Go to the "Control Panel" and open the "Add or Remove Programs" menu.
  • Select "Add/Remove Windows Components".
  • Enable "Internet Information Services" and click "Details".


Fig. 01

2

Installing an FTP server

  • Select "FTP Server (File Transfer Protocol)", "Internet Services Manager" and click "OK". Click "Next" to start the installation of the selected components.


Fig. 02

3 Starting the Internet Services Manager
  • Place your "Windows 2000" CD in the CD drive because it is required for installation.
  • Click "Finish" to close the installation wizard.
  • Start the Internet Services Manager via "Control Panel > Administrative Tools > Internet Services Manager".


Fig. 03

4 Inserting a new FTP site
  • Insert a new FTP site.


Fig. 04

5 Creating an FTP site
  • The installation wizard for the new FTP site is started.
  • Click "Next".
  • Enter a description for your site and click "Next".


Fig. 05

6 Specifying the connection settings
  • Select your computer's IP address, e.g. (192.168.0.1). Enter 21 under TCP port.


Fig. 06

7 Specifying the home directory for the FTP site
  • Enter a home directory for the FTP data.


Fig. 07

8 Access permission to the FTP site
  • Specify the access authorizations for the FTP data.

Fig. 08
9 Opening the properties for the "PanelSite"
  • Click "Finish" to close the installation wizard. A new FTP site is created with the specified settings.
  • Open the properties for the FTP site which you have created.


Fig. 09

10 Granting access
Go to the "Directory Security" tab and enter the panel's IP address (e.g. 192.168.0.10) under "Grant access".


Fig. 10

11 Starting an FTP site
  • Close the "Standard FTP site" by right-clicking and "Close".
  • Start the FTP site which you created by right-clicking and "Start".


Fig. 11

Configuring an Ethernet connection between the PC and the MP370 operator panel
Entry ID 13336639 contains instructions on how to establish a network connection between a PC and a WinCE panel.
The configuration described here involved using the IP address 192.168.0.1 for the PC and the IP address 192.168.0.10 for the panel with the subnet mask 255.255.255.0.

Transferring the Pocket Internet Explorer to the MP370 with ProSave (from V6.0)
So that the Pocket Internet Explorer is available on the operator panel, this option must be transferred to the operator panel with ProSave.
 
No. Procedure
1 Transferring the Pocket Internet Explorer
  • Start ProSave via "Start > Simatic > ProSave > ProSave".
  • Open the "General" tab and select the device type (e.g. "MP370 Touch") and the connection type "Ethernet"; then enter the panel's IP address.
  • Change over to the "Options" tab and check the connection by clicking the "Device status" button.
  • Transfer the Pocket Internet Explorer onto the device by moving the Pocket Internet Explorer option to the pane on the right using the arrow buttons.


Fig. 12

Connecting the panel to the FTP server
In order to establish the connection to the FTP server, you require a folder or file in the FTP directory which is created in the FTP server - see Fig. 07.
 
No. Procedure
1 Starting the Pocket Internet Explorer
  • Start the Pocket Internet Explorer on the operator panel.
  • Enter the following syntax in the address line and click "ENTER" to confirm: ftp://192.168.0.1/ (ftp:// "IP address of the FTP server"/)
    The Pocket Internet Explorer connects to the FTP server.

    Note:
    In order to connect to the FTP server, a folder or file must be created in the home directory for the FTP server.
     
  • Open any file ("Test.txt" in the example) by clicking the link in the Pocket Internet Explorer.

    Note:
    The content of the text file, see Fig. 14, is shown in the Pocket Internet Explorer. Files which cannot be shown in the Pocket Internet Explorer are downloaded directly from the FTP server.


Fig. 13

2 "Opening the Save As dialog window
  • Click the "File" menu and select "Save As...".


Fig. 14

3 Saving a file
  • Select the relevant directory (e.g. "Storage Card2") and assign the file, which is being saved, a file name and extension (e.g. "Test.txt").
  • Click "OK" to save the file.


Fig. 15

Keywords:
Data transmission, Network connection

 Entry ID:15250466   Date:2007-08-15