show the entry list
WinAC MP -- Setting up and parameterizing hardware -- Setting up connections
How in WinAC MP 2008 do you program data transfer with the ET200S 1SI module for the 4-byte or 8-byte communication type?
How can WinAC MP exchange data with a PC or PLC?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Connessione di comunicazione fra ProTool Pro e WinAC Pro tramite Computing (WinAC < V3.0)
Connecting the SIMATIC NET OPC server CD11/2002+SP1 to WinAC MP with PROFIBUS
Connection settings for a communication between ProTool/Pro and WinAC
Connecting ProTool/Pro PC-Runtime with Ethernet to a WinAC MP
ProTool -- Configuring and programming communication -- Configuring communication to S7
Settings in "Status/Force" when using a WinAC MP
Communicating with an S7-200 PLC via PPI using a CP5611 Card with Protool/Pro version 5.10
PPI connection of ProTool/Pro and S7-200
Connecting a ProTool Runtime Panel / PC to an S7 200 via PROFIBUS DP
Connecting a panel to a S7 300/400 controller
Connection settings for a communication between ProTool/Pro and WinAC
How can you increase the performance of HMI devices?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect an operator panel (ProTool) to an H system (S7-400H)?
Connecting a ProTool/Pro Runtime (PC) via Ethernet to an S7-300 or S7-400 station from SIMATIC NET CD 07/2001
ProTool/ProRT and S7-200 with PC/PPI-Cable
Ethernet communication between a ProTool/Pro Runtime (PC) and a CP243-1 (S7-200)
Coupling between ProTool/Pro and WinAC
Coupling between Operator Panel and WinAC Basis/WinAC RTX V4.0
Connection between SIMATIC NET OPC server, ProTool/Pro RT and SIMATIC S7
Connecting an OP as DP slave - configuration of DP direct control buttons
ProTool RT -- Operation and maintenance -- Diagnosing errors
Why are fonts and objects shown moved on a PC Runtime system or operator panel?
$044 transfer error 8 when storing a recipe
Connection settings for a communication between ProTool/Pro and WinAC
Gray border in RUNTIME mode
Defective printing with ProTool Pro Runtime V5.10 under Windows NT
Error message while starting ProTool/Pro Runtime that structure of configuration file "*.fwd" is incompatible.
Error message "GET INSTANCE ERROR" when calling the FWD file
Messages are printed only after the end of runtime
Connection settings for a communication between ProTool/Pro and WinAC
Part number:

QUESTION:
Why do I receive the message "160000 connection to control open-loop control_1 is disconnected" with a connection between ProTool/Pro and WinAC?

Figure 1: Message

ANSWER:
For a connection between WinAC and ProTool/Pro do not switch the operation to "SIMATIC S7 WinAC v6.0", but to "SIMATIC S7-300/400 V6.0".

Connection settings in ProTool/Pro

  • Select "Open-loop control" and doubleclick on your control.
  • Under protocols, select "SIMATIC S7- 300/400 V6.0" and click on "Parameter".

Figure 2: Compile protocol

  • Connect the PC to the WinAC via profibus.

Figure 3: Control connection

Note: 
If you run the WinAC and ProTool/Pro Runtime on two different PCs, the interfaces of both PCs have to be configured at "PG-PC-interface settings"(e.g. settings at WinAC-PC: "WinLC_0 --> CP5611" and at ProTool/Pro Runtime-PC "S7ONLINE --> CP5611 (PROFIBUS)").


 Entry ID:15048936   Date:2003-04-17