show the entry list
ET 200S (standard modules) -- Product information -- Technical data
What are the requirements for using the S7 routing function and which modules can you implement?
Which communication services supported by the CPUs with integrated PROFINET interface and by the WinAC RTX via Industrial Ethernet?
Which PROFIBUS connectors can you use in Zone 1 or 2?
What are the system limits in an F CPU for safe bidirectional data communication via S7 Communication?
Which SIMATIC S7 components and which drives support clock-synchronicity functionality?
ET 200S: Are there special requirements for ET200S when mounted on sheet metal plates?
ET200S: How many motor starters can be allocated to a power module?
ET 200S: How many motor starters can be allocated to a power module?
ET 200S: How many load feeders may be connected?
Calculating the maximum absolute error of the counter module 1Count24V/100kHz (6ES7 138-4DA02-0AB0) when measuring rotational speed
Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gas
Baud rates for ET200S FO modules
Maximum power load for digital output modules
Minimum distance to the ET 200S front
How do you assign and identify thermocouples?
How long does the input signal have to be present before an analog input module identifies this signal as a process alarm?
ET 200S (standard modules) -- Setting up and parameterizing hardware -- Setting up modules for distributed operation
Baud rates for ET200S FO modules
Baud rates for ET200S FO modules
Part number:

QUESTION:
Which PROFIBUS DP baud rates can I use for the communication to my ET200S FO module?

ANSWER:  
The module supports the following baud rates:

  • 12 Mbit/s
  • 1.5 Mbit/s
  • 500 Kbit/s
  • 187 Kbit/s
  • 93.7 Kbit/s
  • 19.2 Kbit/s
  • 9.6 Kbit/s

If you try to set a different baud rate, then in STEP 7 V5.2 you get the error message shown in Fig. 1.

Fig 1: Error message in STEP 7 V5.2

Important:
In STEP 7 V5.1 it is also possible to set transmission rates of 3 Mbit/s and 6 Mbit/s. But these baud rates are not suitable for secure communications.

 Entry ID:15006409   Date:2003-04-14 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour