show the entry list
PROFIBUS general -- Operation and maintenance -- Diagnosing errors
Which diagnostic messages of the DP slave can you read out on a CP342-5 as DP master?
What settings do you make in the Amprolyzer V3.2 to record the messages of a PROFIBUS network and trigger recording on the occurrence of a PROFIBUS event?
With the S7-1200, how do you read out the diagnostics data of a PROFIBUS DP slave with the "DPNRM_DG" instruction and how do you evaluate the data in the user program?
Additional diagnostics address when using DPV1
System requirements for the BT200 log kit
Which organization blocks do you need for error handling?
Questions and answers about Amprolyzer V3.0
PROFIBUS bus monitor AMPROLYZER doesn't run under WIN 98
Testing the availability of a slave with the BT200
Question and Answers on Amprolyzer V3.1
PROFIBUS wiring test BT 200 V2 (MLFB 6ES7181-0AA01-0AA0)
How do you read out the diagnosis data of a PROFIBUS DP slave with the SFC13 "DPNRM_DG" and how do you evaluate the data in the user program?
Report "MS Excel is required" while opening the Amprolyzer
Why is the Diagnostics Repeater recognized in "Accessible Nodes", but not in the Online Hardware?
Commissioning a non-functioning DP master system
Diagnostics tools for commissioning the PROFIBUS DP network
Which organization blocks do you have to load into the CPU to ensure that the CPU does not go into the "STOP" status when a remote I/O fails?
No online connection with STEP 7 after closing Amprolyzer
System requirements for the BT200 log kit
Part number:

QUESTION:
For which operating systems is the log kit suitable?

ANSWER:  
The log kit is for documenting measurements made with the BT200. The log kit can only be used with BT200 from MLFB 6ES7 181-0AA01-0AA0 upwards.

The software supports German, English and French. One of the following operating systems is the requirement:

  • Windows 95
  • Windows 98
  • Windows NT 4.0

Keywords:
Software compatibility

 Entry ID:15005424   Date:2003-04-14 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour