show the entry list
S7-400 CPU 41x -- Setting up and parameterizing hardware -- Initializing and parameterizing modules (GSD, Updates)
How can user-defined web pages and standard web pages be updated automatically in STEP 7 (TIA Portal) V11?
How can you read out the identification data (the serial number of the MMC, for example) with the SFC 51 in STEP 7 V5.5?
Why must you never remove a memory card when the S7-300/S7-400/S7-1200 CPU is in operation (RUN)?
How do you connect the SIMATIC Field PG to the bus system to parameterize and diagnose the distributed I/O devices?
How can time and date be acquired from a GPS signal?
How do you configure time synchronization?
How can you protect the S7-300/400 against unauthorized access from the LAN (local area network)?
What options exist for assigning passwords?
What can you do if new modules, e.g. CPUs, are missing in the STEP 7 module catalog?
What are the conditions for assigning the addresses of I/O modules (central or distributed) to an S7 CPU?
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Where can I procure the GSD files for my S7-400 CPUs?
How do you do a cold start with SIMATIC S7-400 CPUs version V4.0 and higher?
Why should you switch the operating mode of the CPU from Test to Process after commissioning the STEP 7 program?
How do you use or update process image partitions for S7-400 CPU modules during an interrupt OB?
Only up to 27 configured blocks are displayed
What should you watch out for with the "forcing inputs" function in the S7-400?
ET 200S (standard modules) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How do you commission the serial interface module 1SI 3964/ASCII (6ES7138-4DF01-0AB0) in STEP 7 Professional V11 and higher?
How do you commission the serial interface module 1SI MODBUS/USS (6ES7138-4DF11-0AB0) in STEP 7 Professional V11 and higher?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
Why is the message "This page is not available" displayed in the web browser when you call the HTML page "Topology", for example, to read out the topology via the web server of the CPU?
How do you reset the IP address and device name of an I device?
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication in the IWLAN in the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via PROFIBUS in the SIMATIC NET Quick Start Collection?
Where can you find information of the reproducibility of delay interrupts and cyclic interrupts for IM151-8 and IM154-8?
How is reparameterization performed when replacing the IO link master module or the IO link device?
Which options are available for configuring the ET 200 stations?
Where can you find information on installation guidelines for an ET 200S station?
Which diagnostics messages might you get when commissioning the ET 200S as PROFINET IO device?
Which diagnostics messages might you get when commissioning the ET 200S as PROFIBUS DP slave?
TeleService with ET200S (IM151-CPU) and TS Adapter
Can I use a Quickstop function with an ET 200S Motor Starter?
How can you combine fail-safe and standard modules in the ET 200 stations?
Parameterizing ET 200 S DI 4xNAMUR (6ES7 131-4RD00-0AB0)
Temperature compensation of a thermocouple using a resistance thermometer Pt100 to capture the reference junction temperature
Temperature Compensation of a Thermo-element via the Electronic module 2AI TC HF
How can you group the addresses of ET200S IM151-1 HF (pack addresses) in HW Config?
IM 151-7 CPU: Porting Programs with Packed Addresses
How can you group together the address area of the ET 200S (pack addresses)?
Which ET 200S modules support the option handling function?
What conditions do you have to comply with when configuring ET 200S modules?
What should you watch out for regarding the compatibility of I/O modules and interface modules when configuring an ET 200S?
How can you use Bürkert pneumatic modules in the ET 200S remote I/O system?
How can you prevent the bus error LED from lighting on interface module IM 151 when using reserve modules?
ET 200M (standard modules) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
Configuring SIPLUS extreme modules
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication in the IWLAN in the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via PROFIBUS in the SIMATIC NET Quick Start Collection?
Which options are available for configuring the ET 200 stations?
Parameterization data of an analog module in an ET 200 are not transferred when using an external master
Configuring a power supply for an IMxxx in the ET200M
Configuring the Dummy Module => BF in ET200M
Parameterizing the ET200-M (IM153-x) only possible in hex code
The input values of an analog module in the ET 200M sporadically have the value zero
ET200-M with active backplane bus.
Configuring IM153-3 (ET200-M)
"Change of module during operation" parameter option on an ET 200 M
Operating ET200M as slave on master station CPU315-2DP
No startup of ET200M station when using blank slots
"Module change during operation" - Configuration and system requirements
Display of the "Parameter Assignment" tab for the configuration of modules
Output channels of SM 335 do not work
How do you calculate the times for the clock-synchronized operation of ET 200M?
ET 200iSP -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How do you change the PROFIBUS address of the ET 200iSP distributed I/O device and what do you do if the ET 200iSP is not detected via the PROFIBUS address which is set on the interface module?
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Where can you find sample S7 programs and documentation for communication via PROFIBUS in the SIMATIC NET Quick Start Collection?
Which options are available for configuring the ET 200 stations?
Why does the DI (6ES7 131-7RF00-0AB0) on the ET 200 iSP not recognize an input signal?
PROFIBUS S7-300/400 CPs -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Where can you find sample S7 programs and documentation for communication via gateways and network components, and for security in networks on the SIMATIC NET Quick Start Collection?
Master / Slave (SIMOVERT) communication on the DP PROFIBUS
Overall reset of CP443-5 Extended via NCM S7 PROFIBUS Diagnostics
CP443-5 Extended: Loading a configuration with high volume
Inconsistent system data when removing a PROFIBUS DP master system from the network
What should you watch out for when configuring a CP342-5 as DP master and why is it necessary to call the FC1 "DP_SEND" and FC2 "DP_RECV" functions in the user program of the CPU in order to transfer data?
Why are some of the newer versions of the names of SIMATIC NET modules not used in the hardware catalog?
CP 342-5 -- How can you change the PROFIBUS address or the operating mode of the CP 342-5 in running operation?
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Part number:

Configuration Notes
The CiR function (Configuration in RUN) allows system expansion during operation. You can make modifications to plant during operation with CiR in sections of plant with a distributed I/O.

In order to make modifications to plant during operation with CiR you must use one of the modules below as PROFIBUS DP master:

  • Integrated MPI/DP interface or integrated DP interface of an S7-400 CPU
  • External DP master interface CP443-5 EXT from V5.0
  • Interface module IF 964-DP

Using the CiR system you can add or remove compact DP slaves, for example third-party slaves, and the modular DP slaves ET 200M, ET 200iSP and ET 200S to/from an existing PROFIBUS DP master system.

Permissible configuration changes with compact DP slaves
You can add/remove a compact DP slave to/from a PROFIBUS DP master system only as a complete station.

Permissible configuration changes with modular DP slave ET 200M
You can use the CiR function to add/remove the DP slave ET 200M as a complete station to/from a PROFIBUS DP master system. Furthermore, with the modular DP slave ET 200M you can use the CiR function to add and remove individual modules or change their parameters.

Permissible configuration changes with modular DP slave ET 200iSP
You can use the CiR function to add/remove the modular DP slave ET 200iSP as a complete station to/from a PROFIBUS DP master system. In addition, with the modular DP slave ET 200iSP you can use the CiR function to change the parameters of individual modules. You can use the CiR function to replace reserve modules with the coming electronic modules of the ER 200isp.

Permissible configuration changes with the modular DP slave ET 200S
You can use the CiR function to add/remove the modular DP slave ET 200S only as a complete station to/from a PROFIBUS DP master system.
Using the CiR function to add individual modules to the existing modular DP slave ET 200S is not supported to date. If you need additional individual modules in the existing modular DP slave ET 200S, you must first remove the complete station using the CiR function. Then you use the CiR function to add the modular DP slave ET 200S with the additional modules required as a complete station to the PROFIBUS DP master system.
Option handling provides another way of preparing the ET 200S for coming extensions (options). Option handling means, for example, that you assemble, wire and configure the planned maximum configuration of the ET 200S. You can use option handling with or without RESERVE modules.
More information about the Option Handling function with the ET 200S is available in Entry ID: 22564754.

Further Information
More information about the CiR function is available in the manual "SIMATIC STEP7 V5.5 Modifying the System during Operation via CiR" in Entry ID: 45531308.

Information about using the "Configuration in Run" (CiR) function on the PROFINET IO system is available in Entry ID: 49245734.

 Entry ID:14909396   Date:2011-04-27 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour