show the entry list
Multi Panel -- Setting up and parameterizing hardware -- Setting up connections
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Microsoft ActiveSync connection for MP270, MP370
Which hardware can be connected to the USB port on Windows-based panels?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
What connecting cables are there for connections between the operator panels and the different controllers?
How do you connect a panel to a SIMATIC H station?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
How you change / save the size and position of the keyboard on Windows-based operator panels?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
Mobile Panels -- Operation and maintenance -- Setting and operating panels
How you change / save the size and position of the keyboard on Windows-based operator panels?
Starting ProTool Runtime immediately after start-up of the WinCE panel
How can you ensure safe shutting down of the Panel Runtime on a Windows-based operator panel if there is a power failure?
How do you switch an operator panel to transfer mode when the autostart's timeout is set to 0 seconds?
How can you ensure full battery capacity of the Mobile Panel 277 (F) IWLAN even after a long period of time?
Touch Panel / Operator Panel -- Operation and maintenance -- Setting and operating panels
How you change / save the size and position of the keyboard on Windows-based operator panels?
Starting ProTool Runtime immediately after start-up of the WinCE panel
How can you ensure safe shutting down of the Panel Runtime on a Windows-based operator panel if there is a power failure?
How do you switch an operator panel to transfer mode when the autostart's timeout is set to 0 seconds?
Slow blinking of LEDs on the OP37/Pro
Why can you no longer adjust the contrast on Operator Panel OP3?
Influencing background brightness of the Operator Panel OP7
How you change / save the size and position of the keyboard on Windows-based operator panels?
Part number:

Instructions
The size and position of the alphanumerical and numerical keyboard can be set on Windows-based operator panels. The size and position of the alphanumerical keyboard can be saved separately from the settings for the numerical keyboard. The keyboard layout can be changed via the operator panel's Control Panel.

The setting of size and position depends on the Image version of the operator panel. How to proceed for your particular operator panel is given in the "Input Panel" dialog in the "Control Panel" of your operator panel.

Contents

  1. Operator panels with recent Image version
    1.1 Operator panels without "Show Resize button"
    1.2 Operator panels with "Show Resize button"
  2. Operator panels with old Image version

1. Operator panels with recent Image version
There are two different methods for operator panels with a recent Image version. In the case of small displays, the system does not permit you to change the size of the monitor keyboard. The "Show Resize Button" option is not available on these operator panels.

1.1 Operator panels without "Show Resize button"
On these operator panels you can only change and save the position, but not the size.

  • Open the "Control Panel" and click the "InputPanel" icon.
    Icon - InputPanel
     
  • Click on "Open Input Panel".


    Fig. 01
     
  • Drag the window which now appears to the bottom corner of the screen, for example, (although it must still be completely visible). This is so that you can still see and operate this dialog after resizing the keyboard.
  • The keyboard is displayed and you can only change its position (via the keyboard icon at the top right). You cannot change the size of the keyboard.

    Keyboard icon - Change position
     
  • Once you have changed the position, confirm with "Save", followed by "Close Input Panel" to save the settings.
  • Close the dialog box by clicking "OK".

Remark
You can switch between alphanumerical and numerical keyboard mode by clicking the "Num" button on the actual keyboard.

Note
Only the keyboard's alphanumerical view can be saved as power failure-proof. This entails selecting the alphanumerical view before saving. The numerical view cannot be saved as power failure-proof. Following "POWER ON", the size and position of the numerical display is adapted in line with the alphanumerical display.

1.2 Operator panels with "Show Resize button"

  • Open the "Control Panel" and click on the "InputPanel" icon.
    Icon - InputPanel
     
  • Enable the "Show Resize button" checkbox.
  • Click on "Open Input Panel".


    Fig. 02
     
  • Drag the window which now appears to the bottom corner of the screen, for example, (although it must still be completely visible). This is so that you can still see and operate this dialog after resizing the keyboard.
  • The keyboard is displayed and you can change its position (via the keyboard icon at the top right) and size (via the button with the two arrows at the top right).

    Keyboard icon - Change position
    Arrows - Change size
     
  • Once you have changed the size and position, confirm with "Save", followed by "Close Input Panel" to save the settings.
  • Close the dialog box by clicking "OK".

Remark
You can switch between alphanumerical and numerical keyboard mode by clicking the "Num" button on the actual keyboard.

Note
You can save the keyboard's alphanumerical view and numerical view as power failure-proof. Click the "Save" button to save the view selected as power failure-proof.

2. Operator panels with old Image version
There are two different methods for operator panels with an old Image version. In the case of small displays, the system does not permit you to change the size of the monitor keyboard. The function and button with two arrows (see below) are not available on these operator panels.

  • Open the "Control Panel" and click the on the "InputPanel" icon.
    Icon - InputPanel
     
  • Click on "Start Resize".


    Fig. 03
     
  • Drag the window which now appears to the bottom corner of the screen, for example, (although it must still be completely visible). This is so that you can still see and operate this dialog after resizing the keyboard.
  • The keyboard is displayed and you can change its position (via the keyboard icon at the top right) and size (via the button with the two arrows at the top right).

    Keyboard icon - Change position
    Arrows - Change size
     
  • Once you have changed the size and position, click on "Stop Resize" to confirm and then on "Save" to save the settings.
  • Close the dialog box by clicking "OK".

Remark
You can switch between alphanumerical and numerical keyboard mode by clicking the "Num" button on the actual keyboard.

Note
Only the keyboard's alphanumerical view can be saved as power failure-proof. This entails selecting the alphanumerical view before saving. The numerical view cannot be saved as power failure-proof. Following "POWER ON", the size and position of the numerical display is adapted in line with the alphanumerical display.

Additional Keywords
Windows CE 3.0, Windows CE 5.0, Windows CE 6.0

 Entry ID:14787643   Date:2013-05-02 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour