show the entry list
ProTool -- System-wide configuration -- Synchronizing time
How can you calculate the actual local time (summer time or winter time) in the S7-300/400 CPU and then use it on the panel as system time?
How do you synchronize date/time between a line/graphics operator panel (TD17, OP5, OP15, OP17, TP27, OP27, TP37, OP37) and an S7-300/400 controller with ProTool?
How do you synchronize the date and time between a Windows-based operator panel and the S7-300/S7-400 controller with ProTool?
How do you synchronize the date and time between an S7-300/400 and OP3 (C7-621) with ProTool?
How do you synchronize date and time between a TP170A and an S7-300/400 controller with ProTool?
How do you synchronize time/date between a TP170A and an S7-200 CPU with ProTool?
How do you synchronize the date and time between a line or graphics device (TD17, OP5, OP7, OP15, OP17, TP27, OP27, TP37, OP37) and an S7-200 CPU with ProTool?
How do you synchronize the date and time between an OP3 and an S7-200 CPU?
How do you synchronize the system clock between a Windows-based panel and an S7-200 CPU with ProTool?
How are the date and time of the S7-200 CPU displayed on a TP170A connected to it?
How do you synchronize time/date between a SIMATIC HMI panel and a SIMOTION controller?
How does time synchronization work between S5 and a Windows-based operator panel?
STEP 7 Micro/WIN -- System wide configuration -- Synchronizing time
How are the date and time of the S7-200 CPU displayed on a TP170A connected to it?
How do you synchronize date/time between a TP170A / TP170micro / TP177micro and an S7-200 CPU with WinCC flexible?
How do you synchronize the system clock between a Windows-based panel and an S7-200 CPU with WinCC flexible?
How do you synchronize the system clock between a Windows-based panel and an S7-200 CPU with ProTool?
How do you synchronize time/date between a TP170A and an S7-200 CPU with ProTool?
How do you synchronize the date and time between a line or graphics device (TD17, OP5, OP7, OP15, OP17, TP27, OP27, TP37, OP37) and an S7-200 CPU with ProTool?
How do you synchronize the date and time between an OP3 and an S7-200 CPU?
How do you synchronize the date and time between an OP3 and an S7-200 CPU?
Part number:

Instructions:
There are two possibilities for synchronizing date/time between a S7-200 and the OP3:

The communication between the S7-200 and the OP3 is implemented within the interface area that has been entered in the ProTool project.


Fig. 1: Interface area

For time synchronization purposes, the areas control and response bits date and time are relevant.

Transfer date/time from the S7-200 to the OP3 

In the control and response bits area, bit 2 signalized the date/time request of the OP.


Fig. 2: Control/return information bits

The synchronization of the OP 3 with the SIMATIC S7 is carrie out in four steps:

  1. Every 15 minutes the OP 3 sets the bit 2 in the data byte n+0 on 1.
  2. If bit 2 is set, the CPU time has to be read with the function "READ_RTC" from the S7-200 and be copied into the date and time area of the interface area.
  3. As soon as the S7 program resets bit 2, the OP 3 recognizes that the S7 program has stored the current values for time and date in the interface area.
  4. The OP 3 reads out the recent data from data bytes n+15 to n+17 and n+21 to n+24 of the interface area.


Fig. 3: Time/date folder

Transfer date/time from the OP3 to the S7-200
If bit 6 of bytes n+0 of the control and response bit has been set, a new time was set on the OP. If bit 5 of Byte n+0 of the control and response bit is set, the date on the OP was changed. The new values for date and time are stored in the interface area of the date/time folder. For the S7-200, the values have to be copied back into the appropriate variable area and the setting for the CPU time have to be made with the funciton "SET_RTC". Bits 5 and 6 must be reset after setting the CPU clock.

Note:

  • Further information can be found in the manual of the OP3 under entry ID 1142799.

The STEP 7 Micro/WIN library as archive file:
Copy the "timeop3.zip" file into a separate directory and unpack the file. You can then integrate the library, which can be used in version V3.2.2.11 and higher of STEP 7 Micro/WIN, into your S7-200 project.

 Time_OP3.zip ( 2 KB )

Note:
Information on how to insert libraries in STEP 7 Micro/WIN is available in Entry ID 16689345.

 Entry ID:14782704   Date:2009-04-06