Instructions: There are two possibilities for synchronizing date/time between a S7-200 and the OP3:
The communication between the S7-200 and the OP3 is implemented within the interface area that has been entered in the ProTool project.
  Fig. 1: Interface area
For time synchronization purposes, the areas control and response bits date and time are relevant.
Transfer date/time from the S7-200 to the OP3
In the control and response bits area, bit 2 signalized the date/time request of the OP.
  Fig. 2: Control/return information bits
The synchronization of the OP 3 with the SIMATIC S7 is carrie out in four steps:
- Every 15 minutes the OP 3 sets the bit 2 in the data byte n+0 on 1.
- If bit 2 is set, the CPU time has to be read with the function "READ_RTC" from the S7-200 and be copied into the date and time area of the interface area.
- As soon as the S7 program resets bit 2, the OP 3 recognizes that the S7 program has stored the current values for time and date in the interface area.
- The OP 3 reads out the recent data from data bytes n+15 to n+17 and n+21 to n+24 of the interface area.
  Fig. 3: Time/date folder
Transfer date/time from the OP3 to the S7-200 If bit 6 of bytes n+0 of the control and response bit has been set, a new time was set on the OP. If bit 5 of Byte n+0 of the control and response bit is set, the date on the OP was changed. The new values for date and time are stored in the interface area of the date/time folder. For the S7-200, the values have to be copied back into the appropriate variable area and the setting for the CPU time have to be made with the funciton "SET_RTC". Bits 5 and 6 must be reset after setting the CPU clock.
Note:
- Further information can be found in the manual of the OP3 under entry ID 1142799.
The STEP 7 Micro/WIN library as archive file: Copy the "timeop3.zip" file into a separate directory and unpack the file. You can then integrate the library, which can be used in version V3.2.2.11 and higher of STEP 7 Micro/WIN, into your S7-200 project.
Time_OP3.zip ( 2 KB )
Note:
Information on how to insert libraries in STEP 7 Micro/WIN is available in Entry ID 16689345.
|