show the entry list
WinCC -- Creating HMI configurations -- Configuring trends
How many single segments can be connected to the SQL server in PCS 7 or WinCC without impairing performance?
How do you display different trend curves in one picture in WinCC?
How can you change the time range for Online Trend Control during Runtime in WinCC?
How can I remove curve images in the RT mode so that the labeling of the remaining curves follows correctly?
Why, when you select the curve window with the "Read data immediately from archive" option activated, isn't there any data displayed?
Why are not all the values exported with the "Save report" option of the WinCC Online Trend Control?
How do you change the language of the column headers in the WinCC Online Table Control?
How do you export as a CSV file process values displayed in WinCC Online Trend Control?
How can you use a C or VBS script to provide the separate trends of WinCC Online Trend Control with new tags?
How can you trigger recording in the WinCC Online Trend Control?
How can you dynamically configure the time range of the WinCC Online Trend Control via a script?
How can you display archives of other WinCC projects in Runtime?
How do you set the time display format (12-hour or 24-hour) in WinCC Online Trend Control?
How can you change the font size or type of the ruler window?
How is archive data displayed by WinCC Online Trend Control for daylight saving changes?
How can you position the ruler window on the actual value when it opens?
Why are the characters "i" and "u" sometimes displayed with the tag values?
Why are some trends/values not displayed when you zoom?
Why does the WinCC Online Trend Control plot time offset lines in the measured value curves?
How can you shift Trend Control during Runtime?
WinCC -- Configuring Tag Logging -- Parameterizing Tag Logging
How can you increase the timeout for starting and terminating Alarm Logging / Tag Logging?
In WinCC, how can you assign the functions of the toolbar buttons of Online Trend Controls to external buttons?
Why, when you select the curve window with the "Read data immediately from archive" option activated, isn't there any data displayed?
What Smart Tools are there for WinCC?
What are the different types of tags available under licensing law?
Why are archive tags not deleted in the Tag Logging editor ?
What does parameter "Supplying tags" mean for a process tag in Tag Logging?
How can you make changes to the project on the configuration computer while the existing process values continue to be acquired and archived on the customer computer?
How can you set the archiving parameters of multiple archive tags at the same time?
Which changes can be made when configuring WinCC Tag Logging?
How can you achieve archiving cycles of less than 500ms in WinCC Tag Logging?
How can you use process-driven archiving in WinCC for a process tag with SFB37 (AR_SEND)?
How do you use SFB37 (AR_SEND) for process-driven archiving of process values in WinCC Tag Logging archives?
Why, when you select the curve window with the "Read data immediately from archive" option activated, isn't there any data displayed?
Part number:

Description
Up to WinCC V4.02:
the variable names of the archive variables include illegal signs such as ( / ).

As of WinCC V4.02:
if you use quotes ( " ) in the names of the project variables, those variables are not archived in Tag Logging.
Most other special characters are processed. As far as possible do not use any special characters in the names of the project variables. If you do use special characters, then test whether the variables concerned can actually be archived.

There are characters that Tag Logging converts automatically. For example, the Tag Logging editor converts hyphen ( - ) and hash ( # ) to underscore ( _ ).

Keywords
trend configuration

 Entry ID:144365   Date:1999-10-07 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour