|
QUESTION:
What should you watch out for when making a standalone installation
of ProSave V6.0 SP2 when ProSave V6.0 SP2 is installed on the PC as
the first SIMATIC software?
ANSWER:
If you make a standalone installation of ProSave V6.0 SP2 as the
first SIMATIC software on your PC, in the installation setup you
are asked only for a path for shared files of the SIMATIC software
and not for a path for ProSave.
The ProSave path is not offered for selection, because it is
defined in the subfolder "PTProSave"
(C:\Siemens\Common\PTProSave).
The default path setting is "C:\Siemens\Common" and this
setting should also be retained, because this path is valid for the
shared files of all SIMATIC software packages.
If, for example, ProTool or STEP 7 are to be installed later on
this PC, the shared files of the relevant SIMATIC software are
likewise stored in this folder.
Keywords:
Installation directory, Setup
|