show the entry list
Field PG / Power PG -- Operation and maintenance -- Diagnosing errors
Why can you no longer start the STEP 5 software V7.2/V7.23 after the Windows XP security update KB2707511?
How can you improve the boot behavior of SIMATIC IPCs and the SIMATIC Field PG M3?
Why does STEP 7 Basic V10.5 SP2 not recognize the integrated card reader on a notebook or Field PG M3?
Why can't you switch on the WLAN on the SIMATIC Field PG M2 and why doesn't the SIMATIC Field PG M2 close down?
Bluescreen when opening display properties with Windows2000
Why does the touchpad no longer work after connecting a USB mouse to a Field PG running WIN 2000?
Trans PC card in Windows XP
Upon restarting, a driver cannot be loaded because of a conflict with LapLink
After starting up the Power-DVD-Software a Blue Screen appears on the Field PG/Power PG
Why does the Field PG freeze in the case of an S7 Online connection via Wireless LAN?
How can I eliminate the message "ZCfgSvc.exe" when shutting down Windows?
Error message in Windows 2000: restricted virtual memory
Why does the command line not appear under the menu option "Disk Part" when the system is restored during installation?
How can you deactivate the message "A SYNI error occurred in \Device\s7opciax0", which appears each time you start Windows 2000/XP?
Message: COM1 interface cannot be accessed
Touchpad and keyboard do not work any longer
Error message "Unprocessed exception, error number: 0x80070725, Description: incompatible version of the RPC Stub" when deinstalling in Microsoft Windows 2000/NT 4
Communication cannot be started
Why is the error message "\Device\ACPIEC: The hardware of the Embedded Controller (EC) has not responded within the time limit" displayed in the Windows system protocol?
Message: COM1 interface cannot be accessed
Part number:

QUESTION:
Why do I get an error message on my SIMATIC Field PG when I access the COM1 interface via my application?

ANSWER:  
You might have set up a "PC Direct Connection" in your network environment, which is blocking your COM interface.

Please proceed as follows to be able to use the interface again:

Right-click the "Network Environment" icon on your desktop and select "Properties". In the window that opens you see all the network connections and direct connections that are set up on your Field PG. Select all the Incoming Connections and Direct Connections (Fig. 1) and then delete them with the Del key.

Fig. 1: Properties of the network environment.

Open the "Device Manager" via "Start > Settings > Control Panel > System > Hardware". Here, under "Ports (COM & LPT)", you will find the Communications Port (COM1) that you then right-click and deinstall. 

To have the interface recognized again you right-click it in the Device Manager and select the option "Scan for hardware changes". Windows recognizes the COM interface and reinstalls it.

If you have not set up any PC direct connections, then you might not be able to set up any connection. 
In this case too you deinstall the COM interface and then have it recognized anew. 

If after reinstallation you still cannot set up a connection, then please check your computer for the following software:

  • Teleservice software (PC-Anywhere, Real Out, ...)
  • Mobile phone software 
  • Fax software
  • PC card modem (with virtual COM port)

If you do have such software installed, it might happen that this software is blocking communication via the COM interface. You should therefore deinstall the relevant software and then try again to set up a connection.


 Entry ID:14390517   Date:2004-07-29 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour