|
QUESTION:
What should you watch out for when incorporating the Status/Force
in ProTool V6.0 when using a WinAC MP as controller?
ANSWER:
Once you have inserted the "Status/Force" OCX into a ProTool
picture, you are led automatically to the Properties dialog of the
object. For a connection with the WinAC MP, in the "General"
tab you must set "SIMATIC S7 - 300/400" and not
"SIMATIC S7 - WinAC") for the PLC.
Fig. 1: Status/Force setting when using a WinAC MP
|