show the entry list
Mobile Panels -- Product information -- Technical data and ordering information
Wich protective films can I use with SIMATIC HMI panels?
Where are the current declarations of conformity to be found for SIMATIC HMI panels (CE, UL, cUL, GOST)?
What should you watch out for when connecting the equipotential bonding to the connection box of a mobile panel?
How can you determine the "E-Stand" (hardware release) of an operator panel?
What is the power consumption or power dissipation of the SIMATIC HMI operator panels?
Which PROFINET services are supported by SIMATIC panels.
How resistant to chemicals are the SIMATIC Panels and Panel PCs?
What support does Siemens AG offer to make use of panels comply with FDA regulations?
Which panels are certified for shipbuilding?
What should you watch out with regard to licenses for WinCC flexible and panels?
How do you incorporate the execution times of the F blocks for the Mobile Panel 277F IWLAN into the "S7fcotia.xls" table?
Which installation guidelines do you have to watch out for with the transponders for the Mobile Panel 227 IWLAN and the Mobile Panel 277F IWLAN?
Mobile Panel 170 can only be used with the connection box
Which Siemens department holds the EC conformity declarations for SIMATIC HMI?
Which SIMATIC Panels have the CCC certificate?
Which SIMATIC panels have or need an FCC certificate?
No yellow-red emergency stop switch on the Mobile Panel 170
No standard project in WinCE devices
MOBIC -- Product information -- Technical data and ordering information
Which panels are certified for the FM explosion protection standard for North America?
Which SIMATIC panels have or need an FCC certificate?
MOBIC T8: range of a wireless LAN
Which SIMATIC panels have or need an FCC certificate?
Part number:

Configuration Notes
The Federal Communications Commission is an independent US government agency that is responsible for issuing the FCC certificate.


Fig. 01 - Symbol of the FCC certification

The FCC certificate is not required for devices used exclusively in industrial plants.

An FCC certificate is required specially for devices used in the high frequency range. Such devices can be neither sold nor imported in the United States of America without this certification.

The following SIMATIC operator panel has the FCC certificate:

  • Mobic T8
  • Mobile Panel 277 (F) IWLAN

Note
The binding specifications of the certificate are on the back of the device.

 Entry ID:1436211   Date:2010-03-30 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour