show the entry list
F Technology ET 200S -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
What do you have to do when connecting an F-DO (SIMATIC) to an F-DI of the SINAMICS G120?
How can you combine fail-safe and standard modules in the ET 200 stations?
What should you watch out for when using the fail-safe module 4 F-DI/3 F-DO 24V/2A (6ES7 138-4FC00-0AB0) in the central setup with the IM151-7 F-CPU?
Which hardware and software components are necessary for configuring and running a fail-safe ET 200S system?
How do you set the addresses for the fail-safe I/O modules ET 200S and ET 200pro?
ET 200S (standard modules) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How do you commission the serial interface module 1SI 3964/ASCII (6ES7138-4DF01-0AB0) in STEP 7 Professional V11 and higher?
How do you commission the serial interface module 1SI MODBUS/USS (6ES7138-4DF11-0AB0) in STEP 7 Professional V11 and higher?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
Why is the message "This page is not available" displayed in the web browser when you call the HTML page "Topology", for example, to read out the topology via the web server of the CPU?
How do you reset the IP address and device name of an I device?
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication in the IWLAN in the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via PROFIBUS in the SIMATIC NET Quick Start Collection?
Where can you find information of the reproducibility of delay interrupts and cyclic interrupts for IM151-8 and IM154-8?
How is reparameterization performed when replacing the IO link master module or the IO link device?
Which options are available for configuring the ET 200 stations?
Where can you find information on installation guidelines for an ET 200S station?
Which diagnostics messages might you get when commissioning the ET 200S as PROFINET IO device?
Which diagnostics messages might you get when commissioning the ET 200S as PROFIBUS DP slave?
TeleService with ET200S (IM151-CPU) and TS Adapter
Can I use a Quickstop function with an ET 200S Motor Starter?
How can you combine fail-safe and standard modules in the ET 200 stations?
Parameterizing ET 200 S DI 4xNAMUR (6ES7 131-4RD00-0AB0)
Temperature compensation of a thermocouple using a resistance thermometer Pt100 to capture the reference junction temperature
Temperature Compensation of a Thermo-element via the Electronic module 2AI TC HF
How can you group the addresses of ET200S IM151-1 HF (pack addresses) in HW Config?
IM 151-7 CPU: Porting Programs with Packed Addresses
How can you group together the address area of the ET 200S (pack addresses)?
Which ET 200S modules support the option handling function?
What conditions do you have to comply with when configuring ET 200S modules?
What should you watch out for regarding the compatibility of I/O modules and interface modules when configuring an ET 200S?
How can you use Bürkert pneumatic modules in the ET 200S remote I/O system?
How can you prevent the bus error LED from lighting on interface module IM 151 when using reserve modules?
How can you combine fail-safe and standard modules in the ET 200 stations?
Part number:

Description
The following security classes are based on the associated standards:

  • for SIL on IEC 62061 / IEC 61511
  • for PL on ISO 13849-1:2006
  • for category on EN 954-1:1997

Combination of standard and fail-safe modules with ET 200S
If you use the standard output module of the type DC24V/0.5A in combination with power module PM-E F for safe switch-off, you can attain SIL 2PL d/category 3. The standard output modules you can use are given in Entry ID: 39198632.

If you want to have safe switch-off done via a fail-safe output module (F-DO), you can combine standard and fail-safe input/output modules and attain SIL 3/PL e/category 4. However, make sure that you use an appropriate power module PM-E (e.g. 6ES7138-4CB11-0AB0). The SIMATIC Selection Tool (see Entry ID: 26484854) supports you in this.

Combination of standard and fail-safe modules with ET 200M
Refer to the manual "Fail-safe signal modules" (Entry ID 19026151, section 2.3 Configuration with F-SMs in safety mode).
You can also use a combination of fail-safe and standard input/output blocks in an ET 200M station. To attain safety class SIL 3/PL e/category 4 with combined operation in the ET 200M station, you need the isolation module if you are using the following modules of the ET 200M or their predecessor versions.
 
Module Order number
SM326, 24DI, fail-safe 6ES7326-1BK01-0AB0
SM326, 8DI, NAMUR, fail-safe 6ES7326-1RF00-0AB0
SM336, 6AI, fail-safe 6ES7336-1HE00-0AB0
SM326, 10DO, fail-safe 6ES7326-2BF01-0AB0
SM326, 8DO, fail-safe 6ES7326-2BF40-0AB0

The isolation module separates the potential groups of the fail-safe and standard modules. In this case, the standard I/O modules must be slotted to the left and the fail-safe modules to the right of the isolation module.

Warning
The isolation module must also be used for the above-mentioned modules in SIL3/Cat.4/PLe applications as follows:

  • Generally if the F-SMs are used centrally in an S7-300.
  • Generally if the PROFIBUS DP is set up with copper cable.
  • If the PROFIBUS DP is set up with fiber optic cable with IM 153-2FO and you require combined operation of standard and the above-mentioned F-SMs in an ET 200M.

New
The following successor modules can be implemented without isolator module up to SIL3/Cat.4/PLe:
 
Module Order number
SM326, 24DI, fail-safe 6ES7326-1BK02-0AB0
SM336, 6AI, HART, fail-safe 6ES7336-4GE00-0AB0
SM326, 10DO, fail-safe 6ES7326-2BF10-0AB0
SM326, 8DO, fail-safe 6ES7326-2BF41-0AB0

Keywords
Safety Integrated, Mixed operation, PROFIsafe, Distributed Safety mixed operation, Fail-safe, Isolation module, Power module, ET 200 family, DI, DQ, Configuration editor

 Entry ID:14198063   Date:2010-08-09 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour