show the entry list
S7-200 CPUs -- Configuring and programming communication -- Configuring communication to PCs
How do you establish a TeleService connection to an S7-200 via a TC65 terminal as remote modem with PIN transfer by PC/PPI cable?
How should you parameterize a GSM modem to set up a connection from an analog modem for teleservicing an S7-200?
How do you set up a teleservice connection based on MAS 21 to an S7-200 with MD720-3 via STEP 7 Micro/WIN?
How can you graphically display a variable of the PLC via EXCEL as OPC client with PC Access as OPC server?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Communicating with an S7-200 PLC via PPI using a CP5611 Card with Protool/Pro version 5.10
PPI connection of ProTool/Pro and S7-200
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
ProTool/ProRT and S7-200 with PC/PPI-Cable
Why do you get an error message when program downloading in various S7-S7-21x CPUs via USB/PPI or RS-232/ PPI Multi Master cable?
How do you set the network-related parameters for multimaster mode in STEP 7 Micro/WIN?
Which network configuration is typical when implementing the multimaster function?
Which cables do you use for communication in multimaster mode via the COM interface on the PC side?
How can you clear faults in Multimaster mode by parameterizing the COM communications interface on the PC side?
What alternatives are there to connecting to the multimaster network on the PC side?
How can you clear faults in Multimaster mode by parameterizing the COM communications interface on the PC side?
Part number:

 

Preliminary remarks:
Interface problems in Multimaster mode often occur if you are not using one of the two following RS232/PPI cables which you should be using with STEP 7 Micro/WIN as from V3.2 SP4.
 
Product MLFB
Intelligent RS232/PPI cable with built-in RS232/RS485 converter 6ES7 901-3CB30-0XA0
Intelligent USB/PPI cable with built-in USB/RS485 converter 6ES7 901-3DB30-0XA0

If you use the above cables, it provides Multimaster functionality.

Instructions:
Problems in Multimaster mode when using an RS232/PPI cable that are attributable to too long a response time by the COM interface on the PC side can be cleared as follows:
 
Step Procedure
1 Right-click on the "Workstation" icon and then select "Properties".
2 Go to the "Hardware" tab and open "Device Manager".
3 Double-click on "Connections (COM and LPT)" to open the subtab containing the different connections of the PC.
4 Double-click on the port used for PPI communications.
5 In the "Connection Settings" tab select the "Advanced" button.
6 In the dialog box "Advanced settings for COM(X)" you select the lowest values for receive and transfer buffer and then acknowledge with "OK".
7 You must restart the computer to activate the new settings.

Note:
When using Windows NT with a PC/PPI cable, no other masters should be present on the network. So you cannot make the settings described above in Windows NT. In this case you should choose an MPI/PROFIBUS card (see Entry ID: 22634774).

 Entry ID:14015814   Date:2006-02-17 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour