show the entry list
ProTool -- Creating HMI configurations -- Creating pictures
Configuring headers of OP3 pictures in ProTool V5.2 /SP2
Programming the "Set_Bit" function by pressing a button on Windows-based devices
Picture change on the TP170A as tag function
CPU functions for S7-300 with OP7/OP17
Entering an S5TIME" variable in ProTool/Pro to provide values for a timer in the SIMATIC controller
Showing an "S5TIME" variable from a SIMATIC logic control with ProTool/Pro
Configuring the TAB order ProTool
Subsequent insertion of pictures in the configuration
Graying in the OP display of bitmap graphics
Description of the default name "PIC_xx" for a ProTool/Pro screen
Can I also program function keys in the message image?
Special characters and language-specific characters
How can you register unknown ActiveX objects on a PC and then incorporate them in ProTool/Pro?
Settings required for implementation of the ProTool function "Start Program"
Display of help texts for a certain image object on a Touch Panel
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
How do you implement the "Clean Screen" function for cleaning the touch screen on Mobile Panel 170?
How do you configure screen selection on a line or graphics operator panel via controller job 51?
How do you configure screen selection on a Windows-based operator panel via controller job 51?
How can you make a screen selection on an OP3 via the controller?
How can you make a screen selection on a Windows-based operator panel via the controller without using a controller job?
How can you make a screen selection on a Windows-based operator panel by entering a screen number?
How can the display for the danger and warning area of an analog display be made in color?
How can you optimize the response time when changing screens via the controller?
How do you monitor and control tags on panels on which the status/control object is not available?
How can you register unknown ActiveX objects on a PC and then incorporate them in ProTool/Pro?
Part number:

Instructions:
If you copy ActiveX controls onto your PC, you have to make them known in Windows. 

Registering ActiveX controls in Windows

  • Copy the ActiveX control (OCX name.OCX or Name.DLL, in which the ActiveX control is contained) into the directory that you have chosen for this purpose. 
  • Register the ActiveX objects with the command RegSvr32.exe. For this you click "Start > Run" and then enter the following, for example: 
    "Regsvr32 c:\WinNt\System32\MyOCX.ocx".
  • Press "ENTER" for transfer and the name and path of the ActiveX control is entered into the registration database of Windows.

Incorporating an ActiveX control into ProTool/Pro

  • Create a new picture in your PC project.
  • At the bottom edge of the picture is an icon bar (with I/O field, button …). Right-click this and select the menu "Picture elements...".
  • A window opens in which all the registered ActiveX controls of the PC are listed. Set a check mark next to the ActiveX control that is to be incorporated and click "OK".
  • A button has now been added to the icon bar, via which you can insert the ActiveX control into the picture.

Notes:

  • The use of ActiveX controls from other providers can lead to errors (e.g. "memory munchers", performance deterioration, system blockages). The user of the software is liable for any problems when using other ActiveX controls. We recommend that you make thorough tests before implementing other Active X controls.
  • Siemens assumes no guarantee whatsoever for the operation of Active X controls without any conflicts.
  • More information on ActiveX controls and their integration in ProTool is available in Entry ID: 15247601

 Entry ID:13998474   Date:2008-01-21 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour