show the entry list
ProTool RT -- Product information -- General information
What options are there for direct data communication between an FM 357-2 and a panel or Runtime (ProTool, WinCC flexible)?
Which versions of SIMATIC ProTool/Lite, SIMATIC ProTool and SIMATIC ProTool/Pro are compatible with which Windows operating systems?
Buttons and I/O fields on curve windows are not visible in RT (as of V5.1x)
Message indicator continues to be displayed despite counter at zero
Forgotten Superuser password
Function and system keyboard display in runtime
WinCC flexible RT -- Operation and maintenance -- Diagnosing errors
What is the cause of the system error message "260045 The SIMATIC Logon user does not belong to any group or belongs to multiple groups" in WinCC flexible when the user is evidently assigned to just one group?
Message indicator continues to be displayed despite counter at zero
Why are fonts and objects shown shifted on a WinCC flexible PC Runtime system or operator panel?
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
WinCC flexible ES -- Creating HMI configurations -- Configuring alarms and messages
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Message indicator continues to be displayed despite counter at zero
How do you start a sound file via a script in the WinCC flexible PC Runtime?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How can you determine the bit number in WinCC for the "Trigger address", the "Acknowledgement PLC" bit and the "Acknowledgement HMI" bit for creating bit messages?
Which configuration steps have to be taken in SIMOTION SCOUT and WinCC flexible to enable Alarm_S messages and technological alarms to be displayed in WinCC flexible Runtime?
How do you display ALARM_S or ALARM_D messages with process values (so-called associated values) on a WinCC flexible operator panel?
How do you display messages in WinCC flexible?
How can you evaluate the ACK button on a touch operator panel in WinCC flexible?
How can you have system error messages from a SIMATIC S7-300 / 400 displayed in WinCC flexible?
How do you change and display SIMATIC WinCC flexible system events during configuration?
How can you change the ProTool default alarm window setting in WinCC flexible?
How can I acknowledge alarms in WinCC flexible via the PLC?
Why aren't messages output on the event recorder?
Why isn't the "Message display" shown in the foreground, but is covered by picture objects?
Why are no messages from the S7 diagnostics buffer display in WinCC flexible?
How can you get the diagnostics buffer to be displayed in WinCC flexible?
Which settings need to be made in order to display alarm events after a specified point in time?
How can you create messages with externally preset texts as mass data and process them with Excel in WinCC flexible?
Message indicator continues to be displayed despite counter at zero
Part number:

QUESTION:
Why does the message indicator remain displayed even though the counter is at zero?

ANSWER:  

Fig. 1: Message indicator (Meldeindikator) and counter (Zähler)

The message indicator indicates that there are alarm messages to be viewed or acknowledged. The message indicator is displayed whenever an alarm message arrives. 

The message indicator has two states:

  • Flashing: as soon as at least one unacknowledged message is present.
  • Static: when all alarm messages have been acknowledged, but at least one of them has not yet gone.

The counter:

  • Counts up one for each alarm message that arrives
  • Counts down one for each alarm message that goes
  • Is zero when all the errors messages arrived have gone again.

The message indicator disappears when all alarm messages arrived have been acknowledged and gone again.

This property means that the message indicator with a counter state of "zero" can be displayed if a message has arrived, gone, but has not yet been acknowledged.

Keywords:
Message configuration, Message concept

 Entry ID:13911498   Date:2002-12-05 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour