show the entry list
ProTool -- Creating HMI configurations -- Creating pictures
Configuring headers of OP3 pictures in ProTool V5.2 /SP2
Programming the "Set_Bit" function by pressing a button on Windows-based devices
Picture change on the TP170A as tag function
CPU functions for S7-300 with OP7/OP17
Entering an S5TIME" variable in ProTool/Pro to provide values for a timer in the SIMATIC controller
Showing an "S5TIME" variable from a SIMATIC logic control with ProTool/Pro
Configuring the TAB order ProTool
Subsequent insertion of pictures in the configuration
Graying in the OP display of bitmap graphics
Description of the default name "PIC_xx" for a ProTool/Pro screen
Can I also program function keys in the message image?
Special characters and language-specific characters
How can you register unknown ActiveX objects on a PC and then incorporate them in ProTool/Pro?
Settings required for implementation of the ProTool function "Start Program"
Display of help texts for a certain image object on a Touch Panel
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
How do you implement the "Clean Screen" function for cleaning the touch screen on Mobile Panel 170?
How do you configure screen selection on a line or graphics operator panel via controller job 51?
How do you configure screen selection on a Windows-based operator panel via controller job 51?
How can you make a screen selection on an OP3 via the controller?
How can you make a screen selection on a Windows-based operator panel via the controller without using a controller job?
How can you make a screen selection on a Windows-based operator panel by entering a screen number?
How can the display for the danger and warning area of an analog display be made in color?
How can you optimize the response time when changing screens via the controller?
How do you monitor and control tags on panels on which the status/control object is not available?
Settings required for implementation of the ProTool function "Start Program"
Part number:

QUESTION:
Why doesn’t a program enabled with the ProTool function "Start Program" start?

ANSWER:
In rare cases it might that a program enabled with the "Start Program" function does not start.
In the following, remedies are given based on the "MOVITOOLS" program. The procedure is the same for other programs that behave in the same way.

Option 1: Adding parameters to the system variable "Path"

In a ProTool PC project, you must configure the "Start Program" function with the program path as parameter:
e.g. "C:\Programs\SEW\MOVITOOLS\Bin\mtmanagr.exe". 

Furthermore, you must make the following settings on you PC:

  • Open the "Control Panel".
  • Double-click the "System" icon.
  • Switch to the "Advanced" tab and click on the "Environment Variables" button.
  • In the "System variables" field, select the "Path" variable and click on "Edit".

Fig. 1: System variables

  • Now at the end of the "Variable Value" input line you add the path to the program files (DLLs) of the program to be started: ";C:\Programs\SEW\MOVITOOLS\Bin\System".

    Note:
    The value of the "Path" variable contains the path that contains the DLL files for the "MOVITOOLS" program. 

Fig. 2: Editing the system variable

  • Close the dialogs with "OK" and restart your PC.

Option 2: Calling the program via a batch file

In a ProTool/Pro PC project, you configure the "Start Program" function with the path of the batch file as parameter:
e.g. "C:\Movitools.bat". The batch file contains the program call.

Example for the batch file "Movitools.bat" 

// Switch to the drive on which the program is installed 
C:

// Switch to the folder in which the executable program is installed
CD C:\Programs\SEW\MOVITOOLS\Bin

// Program call
mtmanagr.exe

 Entry ID:13884132   Date:2003-03-03