show the entry list
WinCC -- Product information -- Information on WinCC Smart Tools
Compatibility Tool for Automation and Drive Technology
With what are SIMATIC WinCC V7.x, V 6.x and V5.x compatible?
EasyLanguage adds a 'T' to empty ToolTips upon export
Display/mask out first page/final page of the Dynamic wizard
Warning "Object has no or empty type property" when using the Export Wizard
Changing communication between WinCC server and client in WinCC V5 SP2
WinCC Configuration Tool: Error message while reading large WinCC-Projects
How can you make the menu item "WinCC" visible again in MS Excel when using the "WinCC Configuration Tool"?
Presetting the maximum number of lines in the WinCC Configuration Tool
How do you install the WinCC Smart Tools?
What Smart Tools are there for WinCC?
WinCC -- Configuring Tag Logging -- Parameterizing Tag Logging
How can you increase the timeout for starting and terminating Alarm Logging / Tag Logging?
In WinCC, how can you assign the functions of the toolbar buttons of Online Trend Controls to external buttons?
Why, when you select the curve window with the "Read data immediately from archive" option activated, isn't there any data displayed?
What Smart Tools are there for WinCC?
What are the different types of tags available under licensing law?
Why are archive tags not deleted in the Tag Logging editor ?
What does parameter "Supplying tags" mean for a process tag in Tag Logging?
How can you make changes to the project on the configuration computer while the existing process values continue to be acquired and archived on the customer computer?
How can you set the archiving parameters of multiple archive tags at the same time?
Which changes can be made when configuring WinCC Tag Logging?
How can you achieve archiving cycles of less than 500ms in WinCC Tag Logging?
How can you use process-driven archiving in WinCC for a process tag with SFB37 (AR_SEND)?
How do you use SFB37 (AR_SEND) for process-driven archiving of process values in WinCC Tag Logging archives?
WinCC -- Configuring Tag Logging -- Importing and exporting archives
Compatibility Tool for Automation and Drive Technology
Can I save an archive cyclically anywhere?
In WinCC, how can exported archive segments of Alarm Logging or Tag Logging be connected/removed in Runtime?
With what are SIMATIC WinCC V7.x, V 6.x and V5.x compatible?
What Smart Tools are there for WinCC?
What options do you have for exporting a database in SIMATIC WinCC?
Why aren't any files created when exporting curve archives?
What Smart Tools are there for WinCC?
Part number:

Configuration Notes:
A series of Smart Tools are supplied with WinCC. You can find these tools (if installed) by going to "Start > SIMATIC > WinCC > Tools".
In the WinCC Information System (Online Help) you will also find a detailed description under "Smart Tools".

Description:

SmartTools

  • WinCC Configuration Tool
    After installation, help for this tool is available directly in Microsoft Excel under the menu item "WinCC".
    The Configuration Tool is a simple and powerful tool for configuring mass data in WinCC. Microsoft Excel serves as user interface. In this way you can create, import and edit a WinCC project in Microsoft Excel. Here you can use the operating advantages offered to you by Microsoft Excel. You can use the Configuration Tool to configure the data of the Data Manager, Alarm Logging, Tag Logging and the Text Library.
  • WinCC Archive Configuration Tool
    The WinCC Archive Configuration Tool is an Excel add-In. The tool permits simply and powerful configuration of mass data for archiving WinCC process values.
    Here, you can handle quantity frameworks for which the Tag Logging Editor provides insufficient support.
  • WinCC Cross Reference Wizard
    This tool searches all scripts for picture names and tags and extends them such that they can be recognized by the WinCC component "Cross Reference".
    This tool includes the functions of the "Script Upgrade" tool familiar from WinCC V 5.1.
  • WinCC Communication Configurator
    The Communication Configurator was already available in previous versions. In WinCC V6.0 it is assigned to the Smart Tools. Using the Communication Configurator you can adapt the WinCC communication parameters to existing situations in order to ensure an optimum balance between interference susceptibility and connection stability.
  • Registration files OnIOff.reg, OnIOn.reg
    Using these two registration files you can display/hide the button for calling the "WinCC Online Help". With this step you can suppress a Windows operator control.
  • Export/Import Tags
    The program exports all the connections, data structures and tags in corresponding CSV files from an open project. You can then import these into a second project. The CSV format permits you to process the files with a spreadsheet program before importing them again.
  • Tag Simulator
    The tag simulator is used for simulating internal tags and process tags.
    A typical field of application for the tag simulator is testing a configuration without process I/Os being connected, or with process I/Os connected but without the process running. If process I/Os are not connected, you can only simulate internal tags.
    If process I/Os are connected, you can use the tag simulator to supply the process tags directly with values. This permits you to run a function test of the HMI system with the original hardware.
    Another possible field of application for the tag simulator is in producing a project for demonstration purposes. Often there is no system connection available for presenting the HMI system, so here the simulator controls the internal tags.
  • Dynamic Wizard Editor
    You can use the Dynamic Wizard Editor to create your own Dynamic Wizard. Dynamic Wizards are used to automate frequently recurring configuration processes.
  • WinCC Documentation Viewer
    Print jobs of the WinCC logging system can be diverted into a file. In the case of large volumes of data, one file is created for each log page. You can use the WinCC Documentation Viewer to display and print these files.
             

SmartTools up to WinCC V6.x

  • EasyLanguage
    EasyLanguage is a tool for exporting and importing language-dependent objects in and out of process images of WinCC. It helps when creating multilingual pictures by providing the option of translating language-dependent objects outside WinCC. Objects and user objects managed by the WinCC Text Library are not processed by EasyLanguage.

SmartTools up to WinCC V5.x

  • UnlockMultiUse
    In a multiuser system it is possible to configure from different computers. Some editors can only be started once project-wide. If one of these editors is started, then WinCC locks starting of this editor on the other computers of the same project. Once the editor is closed, WinCC automatically releases the lock.
    Now the error case might arise when this lock is not released. The cause of this, for example, could be interruption of the network connections.
    UnlockMultiUse clears such locking situations.
  • ScriptUpgrade
    ScriptUpgrade searches scripts for picture names/tags and upgrades the scripts so that the WinCC Cross Reference component finds the picture names/tags and puts them in the cross-reference list.
  • Redundancy Test Tools: DCOMTest and RtFileView
    DCOMTest:

    For checking the DCOM connection between two computers.
    RtFileView:
    For reading out important redundancy data and checking the aligning procedure of the failure times and aligned measuring points.
  • Address List Import
    Text address lists exported from KOMED (COROS LS-B) or PMCPRO (SIMATIC-S5) can be imported into the WinCC database using Address List Import.
    Address List Import also permits you to edit block access paths in text address lists from PMCPRO (SIMATIC-S5).

Note:
Please also refer to the following entries on the topic of "WinCC Smart Tools":
 
Description Entry ID
How do you install the WinCC Smart Tools? 10880206
With what are SIMATIC WinCC V7.x, V6.x and V5.x compatible? 21927773

Keywords:
Smart Tools

 Entry ID:13681075   Date:2010-05-25 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour