show the entry list
Touch Panel / Operator Panel -- Product information -- Determining performance and quantity frameworks
Which HMI components can you connect with S7-200 CPU and what should you watch out for when doing so?
What are the functional differences between the different SIMATIC panels?
What should you watch out with regard to licenses for WinCC flexible and panels?
Contrast on OP5/15/7/17
Data record loss after transfer of configuration to line OP
No standard project in WinCE devices
Slower reaction times than usual with OP7/17
Configuration of the OP 17 DP 12 with ProTool 2.xx or older version of ProTool
Hardware test on the TP27
Multi Panel -- Product information -- Determining performance and quantity frameworks
Which PROFINET services are supported by SIMATIC panels.
Which HMI components can you connect with S7-200 CPU and what should you watch out for when doing so?
What are the functional differences between the different SIMATIC panels?
What should you watch out with regard to licenses for WinCC flexible and panels?
No standard project in WinCE devices
Mobile Panels -- Product information -- Technical data and ordering information
Wich protective films can I use with SIMATIC HMI panels?
Where are the current declarations of conformity to be found for SIMATIC HMI panels (CE, UL, cUL, GOST)?
What should you watch out for when connecting the equipotential bonding to the connection box of a mobile panel?
How can you determine the "E-Stand" (hardware release) of an operator panel?
What is the power consumption or power dissipation of the SIMATIC HMI operator panels?
Which PROFINET services are supported by SIMATIC panels.
How resistant to chemicals are the SIMATIC Panels and Panel PCs?
What support does Siemens AG offer to make use of panels comply with FDA regulations?
Which panels are certified for shipbuilding?
What should you watch out with regard to licenses for WinCC flexible and panels?
How do you incorporate the execution times of the F blocks for the Mobile Panel 277F IWLAN into the "S7fcotia.xls" table?
Which installation guidelines do you have to watch out for with the transponders for the Mobile Panel 227 IWLAN and the Mobile Panel 277F IWLAN?
Mobile Panel 170 can only be used with the connection box
Which Siemens department holds the EC conformity declarations for SIMATIC HMI?
Which SIMATIC Panels have the CCC certificate?
Which SIMATIC panels have or need an FCC certificate?
No yellow-red emergency stop switch on the Mobile Panel 170
No standard project in WinCE devices
No standard project in WinCE devices
Part number:

QUESTION:
Why are there no standard projects or images for WinCE devices available?

ANSWER:  
In ProTool for WinCE devices, there are no standard projects with corresponding images (Z_System, Z_Passwort, ...) available. 

In these panels, most settings which are used for graphic and line oriented devices in the standard images, are made in the Control Panel. Further functionality for standard images on WinCE devices is implemented by configuring image objects - e.g. message lists, password lists etc.

 Entry ID:13637743   Date:2002-11-14 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour