show the entry list
WinCC -- Setting up development environments -- Parameterizing systems
What should you watch out for when running SIMATIC WinCC or SIMATIC PCS 7 with Microsoft SQL Server 2005 on PCs with multi-core or multiple processors?
How can you change the properties of the ToolTip text (font, font size, ...) in WinCC Runtime?
How can you set up auto logon for SIMATIC IPCs?
WinCC: settings in the pcANYWHERE
Implementing WinCC V5.x on standalone computers (not applicable for V5.1 and higher) with Windows 2000
Symbol bars in the Graphics Designer can no longer be changed in size and location.
WinCC project information is not displayed correctly in the "WinCC Projects" folder in the Windows Explorer
Implementing WinCC V5.x on standalone computers (not applicable for V5.1 and higher) with Windows NT
How do you use the SIMATIC shell to configure the terminal bus of a WinCC station?
Why are WinCC pictures shown incorrectly or with margins in Runtime when using TFT and flat screens?
Which settings must you make in the WinCC-Explorer under "Computer > Properties" on each computer locally?
How can you make "lost" buttons visible again in the toolbar of the WinCC Explorer or the WinCC Graphics Designer?
Why after changing the resolution or installing a second monitor on my computer is the Properties dialog not displayed in the Graphics Designer?
Why are WinCC pictures shown incorrectly or with margins in Runtime when using TFT and flat screens?
Part number:

Description:  
Current TFT monitors are mostly set permanently to a resolution of 1280 x 1024 pixels.

If you want to have WinCC Runtime pictures at full screen size and with full resolution, you must select the following in WinCC: "Computer properties > Graphics Runtime > Window Attributes", and the options "Full Screen" and "Adapt Picture".


Fig. 01
 

Note:
When changing from an analog monitor to a TFT display (Thin Film Transistor) or vice versa, the new display is addressed only after
rebooting the PC. If you change during running operation, the new monitor appears dark.

Keywords:
LCD monitor, LCD display, LCD screen, Flat screen, Resolution

 Entry ID:13411978   Date:2006-11-03 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour