show the entry list
WinCC flexible ES -- Configuring and programming communication -- Configuring communication to PCs
Which settings are required in Windows XP SP2 and WinCC flexible for server-client communication via OPC-DCOM?
How can you use a PC to simulate or realize sending e-mails in the case of an HMI station message?
How do you configure the OPC server PC Access in order to operate WinCC flexible Runtime as OPC client?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Which settings are required in Windows 2000, Windows XP, Windows Vista and WinCC flexible for server-client communication via OPC XML?
Which ports are used by WinCC flexible?
How can you access a Microsoft Windows 2003 server with a panel / PC?
How do you integrate an HMI operator panel into a local network?
What options are there in WinCC flexible for using a Multi Panel or Mobile Panel as an OPC server?
What options are there in WinCC flexible 2004 for using a multipanel as an OPC server?
WinCC flexible RT -- Configuring and programming communication -- Configuring communication to PCs
How do you integrate an HMI operator panel into a local network?
What options are there in WinCC flexible 2004 for using a multipanel as an OPC server?
What options are there in WinCC flexible for using a Multi Panel or Mobile Panel as an OPC server?
How can you access a Microsoft Windows 2003 server with a panel / PC?
How can you use a PC to simulate or realize sending e-mails in the case of an HMI station message?
Multi Panel -- Setting up and parameterizing hardware -- Setting up connections
Which ports are used by WinCC Advanced, WinCC Runtime Advanced, WinCC Runtime Professional, Basic Panels, Comfort Panels, Panels and IPC?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Microsoft ActiveSync connection for MP270, MP370
Which hardware can be connected to the USB port of HMI operating devices?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
What connecting cables are there for connections between the operator panels and the different controllers?
How do you connect a panel to a SIMATIC H station?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
How you change / save the size and position of the keyboard on Windows-based operator panels?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
Touch Panel / Operator Panel -- Setting up and parameterizing hardware -- Setting up connections
Which ports are used by WinCC Advanced, WinCC Runtime Advanced, WinCC Runtime Professional, Basic Panels, Comfort Panels, Panels and IPC?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Which hardware can be connected to the USB port of HMI operating devices?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
How do you connect a panel to a SIMATIC H station?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
What connecting cables are there for connections between the operator panels and the different controllers?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Connection of an OP3 on the MPI interface
OP3 - Transfer mode
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
Mobile Panels -- Setting up and parameterizing hardware -- Setting up connections
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How do you connect a panel to a SIMATIC H station?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Operator controls as DP direct keys on a Mobile Panel 170
Deactivating and Activating of DP Slave Functions on MOBILE Panel 170
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
What connecting cables are there for connections between the operator panels and the different controllers?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
Basic Panels -- Setting up and parameterizing hardware -- Setting up connections
Which ports are used by WinCC Advanced, WinCC Runtime Advanced, WinCC Runtime Professional, Basic Panels, Comfort Panels, Panels and IPC?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How do you integrate an HMI operator panel into a local network?
Which connector cables are available for connecting to SIMATIC Panels?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
WinCC (TIA Portal) -- Configuring and programming communication -- Configuring communication to S7
In WinCC (TIA Portal), how do you configure a connection between WinCC Runtime Advanced or HMI Panel and an S7 controller over Industrial Ethernet (PROFINET)?
How do you configure process-driven archiving for process tags with WinCC Runtime Professional (TIA Portal)?
How do you integrate an HMI operator panel into a local network?
Why does communication not work between WinCC Professional Runtime and S7-1200?
How do you integrate an HMI operator panel into a local network?
Part number:

Instructions
The example below explains how to

  1. Incorporate an operator panel into a local network in order to back up a tag archive to a PC via the local network.
  2. Share a folder or a drive on a PC.
  3. Save a tag archive to a PC via a local network.
  4. Access the files of the Comfort Panel from the PC.

Note
This entry uses a simple example to explain how to integrate an operator panel into a network. Other network constellations are also possible, but these generally require further knowledge of networks.

Attachment 1: Procedure for WinCC (TIA Portal) and Windows 7 ( 668 KB )

Contents
1. Overview
2. Setting Up a Network Connection
    2.1 Assigning a Static IP Address in Microsoft Windows 7
    2.2 Network Configuration on the Operator Panel
    2.3 Additional Settings on the PC
    2.4 Testing the Network Connections
3. Enabling Sharing
4. Saving the Tag Archive
5. Accessing the Files of the Comfort Panel

Attachment 2: Procedure for WinCC flexible and Windows XP ( 1139 KB )

Contents
1. Setting Up a Network Connection
    1.1 Assigning a Fixed IP Address in Microsoft Windows XP
    1.2 Network Configuration on the Operator Panel
    1.3 Additional Settings on the PC
    1.4 Testing the Network Connection
2. Enabling Sharing
3. Saving the Tag Archive

Note
For activating a printer over the network, for example, (see Entry ID: 18720136) addressing must also take place through a "name resolution".

Additional Keywords
GMP, Pharma, Life Science, Validation, FDA 21 CFR Part 11

 

 Entry ID:13336639   Date:2014-07-03