show the entry list
ProTool -- Creating HMI configurations -- Output of protocols, screens, alarm messages and documents
Printed page shifted in the log file with graphic machines and printer EPSON LQ300 
Crash of ProTool/Lite V5.2 SP2 when printing reports
Printing the cross-reference list in ProTool.
Print display list function (images include curves, bars and graphics)
How can you do a report logging, a hard copy or report printing on a printer with Windows-based ProTool panel via HyperTerminal?
Printing with a RMOS Panel via HyperTerminal (serial Data Communication)
What settings do you have to make to be able to print on a network printer with a Windows-based panel (except the 170 series)?
Touch Panel / Operator Panel -- Setting up and parameterizing hardware -- Using additional components
What options are there for direct data communication between an FM 357-2 and a panel or Runtime (ProTool, WinCC flexible)?
What settings are to be made when connecting a printer to a Windows-based panel?
Which can be connected directly to a panel?
Printed page shifted in the log file with graphic machines and printer EPSON LQ300 
How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this?
Floppy disk drive on OP 15, OP 17 and C7-624
How can you switch off the "Sleep" function on Brother printers?
What settings do you have to make to be able to print on a network printer with a Windows-based panel (except the 170 series)?
Cable for loading the configuration onto OP/TP
Connecting two printers to a panel with serial interfaces
Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have?
Printed page shifted in the log file with graphic machines and printer EPSON LQ300 
Part number:

QUESTION:
What are the configurations I have to choose so that the printed page in the log file will be printed correctly with a graphic device and the printer EPSON LQ300? 

ANSWER:  
When logging with a graphic device and printer EPSON LQ300 the  "printpage" will be set ahead for approx. 1 Line. After approx. 15 pages  the printout starts in the page center if endlesspaper is used.

Remedy:
In ProTool the following setup should be used:

  • Under Targetsystem > Printer > Setup  please choose: Choose Printer > duplicate.
  • Enter a name for the printer and select the button "Parameter".
  • In the Parameter of the new printer please add the following string during basic initialisation.:
    ,1bh,28h,55h,01h,00h,0ah,1bh,28h,43h,02h,00h,e0h,10h

This results in a setting for a paperlenght of 12"

 Entry ID:13283546   Date:2002-10-17 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour