|
QUESTION:
What are the configurations I have to choose so that the
printed page in the log file will be printed correctly with a
graphic device and the printer EPSON LQ300?
ANSWER:
When logging with a graphic device and printer EPSON LQ300 the
"printpage" will be set ahead for approx. 1 Line. After approx. 15
pages the printout starts in the page center if endlesspaper is
used.
Remedy:
In ProTool the following setup should be used:
- Under Targetsystem > Printer > Setup please
choose: Choose Printer > duplicate.
- Enter a name for the printer and select the button
"Parameter".
- In the Parameter of the new printer please add the following
string during basic initialisation.:
,1bh,28h,55h,01h,00h,0ah,1bh,28h,43h,02h,00h,e0h,10h
This results in a setting for a paperlenght of 12"
|