|
QUESTION:
Why do I receive the BATCH flexible message "Invalid
project name"?
ANSWER:
In a BATCH flexible environment, all WinNT stations on which
BATCH flexible is used, have to be equipped with the same
user names with identical passwords. The users must have at least
main user rights in the process or the configuration phase. As is
the case with all other components of the PCS 7 software, the
installation of the BATCH flexible Software Windows NT has
to be done with administrator rights.
Keywords:
User Administrator, rights assignment, installation
|