|
QUESTION:
What are the order numbers for crimp contacts/tools for the
front connector of the S7-400?
ANSWER:
Crimp contacts for the front contactors for S7-400 and the relevant
tools have the following order numbers:
|
Order number
|
Ordering data
|
|
6XX3070, 250 pcs
|
Crimp contacts
|
|
6ES5 497-8MA11
|
Unlocking tool for crimp contacts (for S5 and S7)
|
|
6ES5 497-4UC11
|
Unlocking tool for crimp contacts (for S5)
|
|
6XX3071
|
Crimping tool
|
Table 1: Order numbers
Note:
The crimp contacts can also be used for S5 modules. The tools are
needed in case of a change to remove contacts already mounted in a
connector or to connect the contacts to the cables.
Fig. 1: S7/S5 tool
Fig. 2: S5 tool
Notes on how to employ the unlocking tool for crimp
contacts:
Take the front connector and first remove the cover. Unlocking is
always down from the cable connection side that has now been made
free. Under the pin designation of each contact next to each
contact cavity there is a small slit going off to the right. Insert
the unlocking tool with its metal lug into this slit.
The position of the tool is such that the longitudinal indentation
on the narrow side of the grip faces the cavity wall. The cable
coming away from the crimp contact is laid in this indentation. Now
you push the tool into the slit as far as it can go. This unlocks
the contact and at the same time it is pulled back out of the
cavity with the cable and tool.
If the contact has been pushed into the cavity incorrectly without
a crimped cable and has to be pulled out again, then you must use a
screwdriver, for example, to push from the front so that the cable
is released from the cavity.
|