show the entry list
S7-300 Cables and Accessories -- Product information -- Technical data
Which SITOP power supply can you use for recharging lead batteries?
Where can you find information about the S7-300/400 backup batteries?
How can you prevent your power supply from being cut off unintentionally because of switch-on current peaks that are too high?
How can you prevent failure of a SIMATIC S7 CPU when another 24V power consumer on a common power supply causes a short-circuit?
Which front connector do you need for S7-300 analog/digital modules and for S7-300 compact CPUs?
Which front doors for S7-300 modules can you use in particular when using a 40-pin front connector?
What are the order numbers of the back-up batteries for the various CPUs?
Why are no MTBF values given for the S7-300 front connector?
Current Node - Line filter B84102-K40
Where can I find the current order numbers for converted sensor lines?
Notes for the use of printers intended for the printing of label stripes
Where can I find the current order numbers for converted sensor lines?
Part number:

Description
The following table shows the order numbers for sensor lines for various modules which have an interface for reading in sensors. The table contains also information about the length of the converted sensor lines.

Sensor_cable_e.pdf ( 389 KB )

 Entry ID:12663106   Date:2012-05-23 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour