show the entry list
AS-Interface System Components and Accessories -- Setting up and parameterizing hardware -- Connecting and wiring devices
3SF5874 AS-i-Front Panel Modules: Connection of AS-i- and auxiliary voltage
Is it possible to use AS-Interface motor starters in circuits fed by frequency convertors?
3SF5874 AS-i-Front Panel Modules: Connection of AS-i- and auxiliary voltage
Part number:

QUESTION:

How are the AS-Interface front panel modules usually delivered?
With a connection possibility to AS-i (yellow cable) and external power supply (black cable)?

On the back there are 2 connections but the connection for the external power supply does not have any penetration contacts. Why? Does that depend on the AS-Interface communication module used internally?


ANSWER:

The 3SF5874-4 AS-Interface front panel modules are always delivered without a connection for the external auxiliary voltage.
Only the yellow cable must be connected.
The yellow cable supplies the lamps with voltage.

 

 Entry ID:12281487   Date:2012-03-09 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour