show the entry list
Industrial Ethernet S7-300/400 CPs -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
What should you watch out for when a MAC address is entered for the PROFINET interface or GBIT interface in the configuration of the Industrial Ethernet CP343-1/CP443-1?
How do you configure a shared device when you are using a CPx43-1 Advanced as PROFINET IO controller and the GBIT interface of the module is networked?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
Which Industrial Ethernet CPs support the DHCP Option 12 (Host Name) and how do you configure the DHCP Option 12?
What should you watch out for when parameterizing the watchdog time when a ring redundancy is established with the Media Redundancy Protocol?
How do you use an Industrial Ethernet CP or SCALANCE S as a gateway?
How do you disable the "Link Layer Discovery Protocol" function at the ports of an IE CP of S7-300 or S7-400?
Where can you find sample S7 programs and documentation for communication via gateways and network components, and for security in networks on the SIMATIC NET Quick Start Collection?
What should you watch out for when operating a CP443-1EX20 V2.0 on a CPU V5.1?
Changing the configuration data of users for CP 343-1 IT and CP 443-1 IT
Loading the configuration via LAN into the IE-CP in "STOP" mode
Special points when setting the LAN medium for Industrial Ethernet CPs
Starting up automation systems with Industrial Ethernet without previous node initiation via MPI
Rejected diagnostics connection via TCP/IP protocol after changing the MAC address
Establishing an online connection to an S7-300/S7-400 CPU through several Ethernet interfaces
What should you pay attention to when formatting the file system in the S7-300 and S7-400 Industrial Ethernet CPs?
What should you watch out for when replacing the CP443-1 (6GK7443-1EX11-0XE0) with a CP443-1 (6GK7443-1EX20-0XE0 V1.0) in STEP 7 V5.4 SP3?
What is the meaning of the configuration option "Activate Web server" with CP443-1 EX20?
Why with CP443-1 Advanced is a different firmware version than the module displayed in the C-PLUG info text in the NCM S7 Diagnostics?
Which options are available for assigning the PROFINET IO controller a new IP address?
How can you configure an S7 CP during runtime?
How do you disable the S7 routing functions?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
How can you protect the S7-300/400 against unauthorized access from the LAN (local area network)?
What should you watch out for when using the function block FB55 "IP_CONFIG" to configure an Industrial Ethernet CP?
Why are some of the newer versions of the names of SIMATIC NET modules not used in the hardware catalog?
Why can't my SIMATIC S7-300 Ethernet CP run as many S7 communication connections as specified?
How does connection multiplexing work and how do you configure it for SIMATIC S7-300 Ethernet CPs?
Starting up automation systems with Industrial Ethernet without previous node initiation via MPI
Part number:

QUESTION:
Can automation systems be started up only via IE?

ANSWER:
Under certain circumstances it is possible to start up automation systems exclusively via IE. Node initiation via MPI is then no longer necessary.

Hardware requirements:

  • Automation system S7-300 or S7-400 with IE CP 
  • PG/PC/Notebook with Ethernet network cared (e.g. CP1612, CP1613, etc.) 

The following CPs with IE interface can be used:

  • CP343-1 with EX11 release 02 and higher, FW 2.0.0, at least STEP 7 V5.1+SP2 
  • CP343-1 IT with GX11 release 01 and higher, FW 2.0.7, at least STEP 7 V5.1 +SP3
  • CP443-1 with 6GK7 443-1EX11-0XE0 release 3 and higher, FW V2.0
  • CP443-1 IT with 6GK7 443-1GX11-0XE0 release 2 and higher, FW V2.0

Software requirements:

  • STEP 7 with NCM S7 for IE and SOFTNET-PG. Remark: STEP 7 includes NCM  in versions STEP 7 V 5.x and higher. 
  • PC with LAN connection, ISO protocol must be installed (the S7ONLINE access point must be assigned to this).

Function:
At the "Initial Startup" via IE, the controller system is addressed via the MAC address of the CP. The Ethernet CPs are provided in the works with a unique MAC address, which is printed on the modules and must be entered when configuring the CP. In the case of addressing via MAC address, you must make sure that S7ONLINE access point is set to "ISO protocol". You do this setting in the SIMATIC Manager:

  Fig. 1 ( 36 KB )  

In this example the following configuration has been selected:

  • Rack CR3
  • PS 405, 4A
  • CPU416-2 DP
  • CP443-1 IT

Note:
The modules are taken directly out of the original packaging and are not configured!

There are in principle several options for starting up an automation system for the first time via IE:

  •  Via direct connection between CP and PC (STEP 7 is installed on the PC): 
The twisted-pair cable connects the J45 connections of the CP with the Ethernet network card of the PC. In the case of direct connections, you must use a crossed twisted-pair cable.
  • Via a LAN:
The CP is connected with the STEP 7 PC via an active network component (e.g. hub, switch bridge) via a twisted-pair cable. Routers cannot be used for initial addressing.

Below are the configuration steps for initial startup of the above-mentioned system illustrated with screen shots. 

  1.  Create an S7 project and the hardware configuration, open the Properties dialog for parameterizing the CP and select the properties:
  Fig. 2 ( 41 KB )  
  1. In the Properties dialog you must enter the MAC address printed on the CP in the works (2a). Here via the subnetwork mask you can also define the IP address for later addressing via TCP/IP. The initial addressing of the module however must be done via the MAC address. The CP must still first be networked (2b).
Fig. 3 ( 42 KB )  
  1. Checking that the CP is networked:
Fig. 4 ( 41 KB )  
  1. Saving and compiling the hardware configuration (generation of the SDB):
Fig. 5 ( 38 KB )  
  1. Loading the configuration into the controller. There is a display of the address the PC uses to connect to the CPU: the CP is connected to the CPU via the backplane bus.
Fig. 6 ( 41 KB )  
  1. Loading the system data deletes the data blocks generated in the CPU by SFC. Acknowledge this procedure positively. >
  2. During loading the CPU is set to STOP and the system queries whether the module should run a restart. Acknowledge this procedure positively.
  3. Whilst the module is being restarted, for the initial addressing via IE, you have the following system behavior: the connection between CP and PC clears down for a short time. This connection clear-down is shown in the task bar.>
Fig. 7 ( 74 KB )  
  1. After a short time the connection sets up again. Repeat the procedure. The hardware configuration is then loaded successfully. The LED displays of the automation system light green.
Fig. 8  ( 45 KB )  

Note:
This system behavior occurs in automation systems in which the CP is connected directly with the STEP 7 PC. This only happens the very first time the hardware configuration is loaded via CP using IE. The modules are original modules straight from the packaging without any previous configuration. If there is already a configuration on the automation system, this system behavior does not occur.

 Entry ID:12093514   Date:2002-07-04 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour