show the entry list
S7-400 Cables and Accessories -- Product information -- Technical data
Where do you procure labeling strips and wiring diagrams for S7-400 I/O modules?
S5 modules that can be implemented in the S7-400 system using the adapter
Where can you find information about the S7-300/400 backup batteries?
Why is a battery fault signaled when you insert a back-up battery, even though the battery is new?
What is the effect of the 1 Batt./OFF/2 Batt. settings on the BATT.INDIC switch?
How great is the power requirement (from the backup battery) of the modules to be backed up at "Power Off" and what is the relationship between the backup current and the length of the backup time?
When should you replace the back-up battery on your S7 300/400 controller?
What are the order numbers of the back-up batteries for the various CPUs?
S7-300 Cables and Accessories -- Product information -- Technical data
Which SITOP power supply can you use for recharging lead batteries?
Where can you find information about the S7-300/400 backup batteries?
How can you prevent your power supply from being cut off unintentionally because of switch-on current peaks that are too high?
How can you prevent failure of a SIMATIC S7 CPU when another 24V power consumer on a common power supply causes a short-circuit?
Which front connector do you need for S7-300 analog/digital modules and for S7-300 compact CPUs?
Which front doors for S7-300 modules can you use in particular when using a 40-pin front connector?
What are the order numbers of the back-up batteries for the various CPUs?
Why are no MTBF values given for the S7-300 front connector?
Current Node - Line filter B84102-K40
Where can I find the current order numbers for converted sensor lines?
Notes for the use of printers intended for the printing of label stripes
Where can you find information about the S7-300/400 backup batteries?
Part number:

Description
The data sheets and latest transport regulations for the backup batteries are available for downloading on the Internet sites of the manufacturers.
 
Order no. Manufacturer designation used in Internet site
6ES7971-1AA00-0AA0 SB-AA02(P)
(Vitzro Cell)
S7-300 www.vitzrocell.com
LS 14250
(SAFT)
www.saftbatteries.com
6ES7971-0BA00 SL 360
(Tadiran)
S7-400 www.tadiranbatteries.de/eng/home/

These lithium batteries comply with the special regulation 188 / Part 2 PI 968-970.
 
Order no. Certificates / Documents
6ES7971-1AA00-0AA0 Product_Data_Sheet_Vitzrocell.pdf ( 165 KB )
SB-AA02(P).pdf ( 110 KB )
LS 14250.pdf ( 268 KB )
6ES7971-0BA00 SL 360.pdf ( 37 KB )
Tadiran_Safety_data_sheet_e.pdf ( 58 KB )

 Entry ID:12067424   Date:2012-10-09 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour