show the entry list
Option PDM -- Working with projects -- Creating and editing projects
How do you use the different versions of SIMATIC PDM to access the devices that can be configured with SIMATIC PDM?
Loading Siprom projects
Transferring parameters from SIPART controllers on the SIPART DR net to SIPART controllers on the PROFIBUS DP net
Changing the address of a PA exchange device with SIMATIC PDM V5
Device assignment SIMATIC PDM up to V5.2
How can I incorporate ready-parameterized field devices from my Project A in a different Project B?
What are the requirements for using SIMATIC PDM Data Record Routing?
When is it possible to change a field device address?
How are HART field devices installed in the HW Config?
Why are there not any PDM devices available after you install SIMATIC PDM?
How do you use the HART secondary variables in addition to the actual HART process value in PCS 7?
How can I communicate with PDM (Process Device Manager) under Windows 2000 /XP Professional via the serial interface?
Working with Non-integrated Field Devices in SIMATIC PDM V5.1 through V5.2+SP1
Removing Devices in Network View in SIMATIC PCS 7 V6
How are PROFIBUS PA devices configured in PCS 7 V6.1 HW Config - and then in SIMATIC PDM V6.0 if the device first has to be imported into both configuration tools?
What should you do if devices which are imported subsequently are not displayed in the SIMATIC PDM device catalog (starting with PDM V6.0)?
What procedure should you follow if not all PA field devices are interconnected by the CFC driver wizard starting with PCS 7 V6.1?
How do you integrate devices into the SIMATIC PDM V6.0 at a later date?
Configuring field devices with SIMATIC PDM V5.2+SP1 and Hardware Configuration in PCS 7 V6.0
How do I configure and parameterize an ET 200iS with PCS 7 and PDM?
When is it possible to change a field device address?
Part number:

QUESTION:
Why can’t I change the address of my field device?

ANSWER:  
You are using a PROFIBUS DP device or a PROFIBUS PA device and in PDM want to change the address of your field device via the function "Assign Address" (Menu > Device > Assign Address).

Changing the address depends on different factors:

  • In cyclic mode it is not permissible to change the address by definition. However, this function is not implemented in all devices.
Remedy:
Before changing the address load the HW configuration with the changed address into your CPU. Upon restart the device is no longer on the parameterized address and thus no longer in the cyclic mode. Now it is possible to change the address.
  • The device must be able to manage address on the software side.
  • Devices that can manage the addresses from the hardware and software side must be set to software-side management. This setting can be changed by a parameter or via a DIP switch. Information on this is available in your field device documentation.
  • The DD (Device Description) must support changing of addresses. If the DD does not support this function, then the entry "Assign Address" is missing from the PDM menu item "Device".
  • The CP 443-5 EXT does not support the "GetSlaveAddress" service required for changing addresses. This is why DP slaves that are directly on the DP segment of the CP cannot be reparameterized. Changing the address of a PA field device behind a standalone DP/PA coupler is also not possible. (It is possible to change the address behind a DP/PA link with DP/PA coupler).
    Here you can only change the address only from the PG/PC via CPs 5611 and 5613 with direct connection to this DP segment.
    Note:
    With SIMOCODE DP, the address is changed via a special path. This makes it possible to also change the address through the CP 443-5.

 

 Entry ID:11868716   Date:2002-06-21 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour