show the entry list
WinCC -- Working with projects -- Creating and editing projects
How can you tell the version with which a WinCC project was last processed?
How can you prevent operations or value changes being made simultaneously by multiple WinCC clients?
How do you use a monitor with a 1680x1050 pixel resolution with the OS project editor in WinCC?
How do you integrate an existing WinCC project into a STEP 7 project?
How do you activate access protection for a STEP 7 project and set up a user as project editor?
How do you rename WinCC projects?
In WinCC, how do you activate and deactivate the global color and global shadow for all objects in a picture?
How can you reduce the size of the transaction file (*.LDF) of the database of a WinCC project?
Change the name of a project in the database
Setting configuration to "not activated" in the database
What should you watch out for in particular when using the WinCC Project Duplicator with downtime monitors and process monitors?
What options does the WinCC Project Duplicator provide for creating a redundant server project?
Why can no OS be inserted in the SIMATIC Manager when using STEP 7 V5.2 and WinCC V5.1?
What should you watch out for when duplicating a project from a multi-client computer to another multi-client computer?
How can you use other mouse pointers than the ones set by default in WinCC V5.x Runtime?
How can you dynamize your mouse pointers from SIMATIC WinCC?
How can you use user defined colors from an existing WinCC project in another or a new WinCC project?
Modifying the color of the RT- cursor
Which criteria apply to the name of a WinCC project?
STEP 7 -- Working with projects -- Creating and editing projects
How do you compare blocks in a multiproject?
What are the requirements for migrating a STEP 7 V5.x project to STEP 7 Professional (TIA Portal)?
How do you link a self-made online help to a programmed block in STEP 7 V5.x?
How do you display the diagnostics buffer of a SIMATIC CPU with integrated web server on a SIMATIC Panel?
How do you install the improved block protection for FBs and FCs in STEP 7 V5.5 onwards?
In STEP 7 V5.x, why can the "Find/Replace" dialog not be displayed in the LAD/STL/FBD editor?
How do you integrate a WinCC flexible project in STEP 7?
How can you improve the performance in the SIMATIC Manager and in the STEP 7 project?
Why can you no longer choose the options (Display, Filter, Generate, Delete) in the menu item "Tools > Reference data >"?
How do you save a STEP 7 project as read-protected on an MMC in an S7-300 CPU?
How do you activate access protection for a STEP 7 project and set up a user as project editor?
How do you update the STEP 7 hardware catalog in STEP 7 V5.2 onwards?
How can you load projects to a memory card and back again to a PG/PC?
Information about "Loading and testing programs"
How do you integrate an existing WinCC project into a STEP 7 project?
What are the advantages of the "Multiproject" function for large networked projects?
What is the significance of the initial and actual values of a data block?
Why can projects, blocks or the HW Config either not be opened at all or only opened with error messages or only as "read only"?
WinCC -- Configuring and programming communication -- Communication to S7 (without PROFIBUS)
How do you integrate an existing WinCC project into a STEP 7 project?
Can I use the Slot PLC with WinCC V5.0?
What are the requirements for an online connection between WinCC and an S7 with MPI (CP5611)?
Which license do you need for communication via TCP/IP with WinCC?
What are the options for accessing an S7-200 with WinCC?
How do you set up a link via modem to an S7?
How can you link WinCC to S7 PLCSIM?
Which settings have to be made in WinCC to communicate with an S7 controller via the TS Adapter?
Which hardware and software is required in the WinCC system to communicate with an S7 via a CP343-1?
Which settings are required to access an S7 CPU with WinCC and SIMATIC NET via a CP5611, CP5613 or CP1613?
How do you integrate an existing WinCC project into a STEP 7 project?
Part number:

Configuration Notes
The following WinCC components must be installed to be able to import a WinCC project into a STEP 7 project:

  • SIMATIC Device Drivers
  • Object Manager 
  • AS-OS Engineering

These components are on the WinCC Installation CD (Fig. 01). Furthermore, WinCC and STEP 7 have to be installed on the same computer. By importing the WinCC project into a STEP 7 project you can use the existing compression tool (packer) for archiving the WinCC project.


Fig. 01

Note
More information on installing additional components (taking the example of "Smart Tools") in different versions of WinCC is available in Entry ID: 10880206 .

Instructions
You have the following options for importing a previously separate WinCC project into your STEP 7 project:

1. Procedure for WinCC V6.0 SP4 and higher
 
No. Procedure
1 In the SIMATIC Manager you execute the menu command "Options > OS Import...".


Fig. 02

2 Press the button marked to open the selection window shown in Fig. 04.


Fig. 03

3 Select the Projectname.mcp file that you wish to import and press the "Open" button.


Fig. 04

4 Check the project path for the OS to be imported and press the "Import OS" button.


Fig. 05

Note
More information on importing WinCC projects with the SIMATIC Manager is available in the WinCC Information System > Working with WinCC > The Integration of WinCC in SIMATIC Manger > Managing WinCC Projects and Objects with SIMATIC Manager > Importing a WinCC Project with SIMATIC Manager.

2. General procedure for all versions of WinCC
 
No. Procedure
1 Insert an Operator Station (OS) into your STEP 7 project.


Fig. 06

2 Change the name of the OS to the one in your WinCC project.


Fig. 07

3 In the Windows Explorer, delete the WinCC project created in the STEP 7 project path, which is generated because of the newly created OS. 
Sample project path: 
C:\Programs\Siemens\Step7\EXAMPLES\exie\wincproj\'Name of the OS'
4 Now store the existing WinCC project in the STEP 7 project path using the Project Duplicator via the menu item "Save as...". You start the Project Duplicator in the Start menu under "Start > Simatic > WinCC > Tools".

Note
More information on importing WinCC projects with the SIMATIC Manager is available in the WinCC Information System > Working with WinCC > The Integration of WinCC in SIMATIC Manger > Managing WinCC Projects and Objects with SIMATIC Manager > Importing a WinCC Project with SIMATIC Manager.

Creation environment
The instructions in this entry were created in the following environment.
 
Component Product and version designation
PC operating system Microsoft Server 2003 SP2
Standard tools STEP 7 V5.4 SP4
HMI software WinCC 7.0
Options ---
Controllers ---

 Entry ID:11841504   Date:2010-05-17 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour